Fetch failure for URL 'git://sw-stash.freescale.net'

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fetch failure for URL 'git://sw-stash.freescale.net'

2,252 次查看
mdanilau
Contributor I

Hi,

I'm trying to rebuild the linux kernel for LS1021A with QorIQ-SDK-V1.8.

With 'bitbake -c menuconfig virtual/kernel' i deactivated all freescale network kernel drivers and activated AX88772A network driver.

Duting executing 'bitbake virtual/kernel' i get errors like

...

ERROR: Fetcher failure: Fetch command failed with exit code 128, output:

Cloning into bare repository '/home/mdu/Freescale-Linux-SDK-for-LS1021A-Rev2-v0.4-20150803-yocto/sources/git2/sw-stash.freescale.net.scm.dnnpi.ls1-linux.git'...

fatal: unable to access 'http://sw-stash.freescale.net/scm/dnnpi/ls1-linux.git/': Could not resolve host: sw-stash.freescale.net

ERROR: Function failed: Fetcher failure for URL: 'git://sw-stash.freescale.net/scm/dnnpi/ls1-linux.git;branch=LS1-SDK-Rev2.0;protocol=http'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/mdu/Freescale-Linux-SDK-for-LS1021A-Rev2-v0.4-20150803-yocto/build_ls1021atwr_release/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-ls1/3.12-r0/temp/log.do_fetch.18550

ERROR: Task 2 (/home/mdu/Freescale-Linux-SDK-for-LS1021A-Rev2-v0.4-20150803-yocto/meta-fsl-arm/recipes-kernel/linux/linux-ls1_3.12.bb, do_fetch) failed with exit code '1'

...

The question is: what i'm doing wrong?

标签 (1)
0 项奖励
回复
0 回复数