FRDM-LS1012a prebuilt images

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-LS1012a prebuilt images

2,711 Views
abhilashvr
Contributor II

Hi All,

Trying to update FRDM-LS1012a reference board with prebuilt images.

Based on Getting started page of FRDM-LS1012a , Downloaded Image: QorIQ Linux SDK v2.0 AARCH64 IMAGE.

But that only contains LS1043ARDB, LS2080ARDB images, No prebuilt image for FRDM-LS1012a. Attaching the screen shot of the Folders in the mounted images.

Could some one please point me to the  FRDM prebuilt image location ?

Thanks

Abhilash

Labels (1)
0 Kudos
Reply
1 Reply

2,315 Views
Pavel
NXP Employee
NXP Employee

The SDK 2.0 supports the FRDM-LS1012a board if QorIQ Linux SDK v2.0-1703 update is installed. If this update is installed, SDK 2.0 provides building image for the FRDM-LS1012a board.

Use LSDK for loading prebuilt image for the FRDM-LS1012a board:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply