FRDM LS1012A SDK problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM LS1012A SDK problem

1,373件の閲覧回数
13540372905
Contributor I

As we mentioned before about the SDK of FRDM LS1012A, we received a reply that sdk-1703 supports the board, but according to the link, only the corresponding installation package was not found. Please help provide an SDK package download link that supports the board of FRDM LS1012A,thank  you!

0 件の賞賛
返信
1 返信

1,308件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello liu xin,

Please login in www.nxp.com , download Linux SDK 2.0 from Linux® SDK for QorIQ® Processors | NXP .

Please download and install the following ISOs.

Source: QorIQ Linux SDK v2.0

Update: QorIQ Linux SDK v2.0-1703

Cache: QorIQ Linux SDK v2.0 AARCH64 Yocto


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信