FPGA configuring with LS1043

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FPGA configuring with LS1043

ソリューションへジャンプ
2,027件の閲覧回数
AntoNico10
Contributor II

Hello everyone,

I'm planning to use the NXP LS1043 processor for a project that involves configuring a Xilinx Kintex UltraScale+ FPGA through the Passive Serial (PS) configuration mode. I'm curious about the feasibility of this setup and have a couple of questions:

  1. Is it possible to configure the Xilinx Kintex UltraScale+ FPGA via Passive Serial using the LS1043 processor?
  2. For the configuration process, can I use generic I/O pins on the LS1043, or are there specific pins that I need to utilize for this purpose?

Any insights or guidance on how to achieve this configuration would be greatly appreciated. If anyone has experience with a similar setup or can provide documentation or examples, that would be extremely helpful.

Thank you in advance for your assistance!

0 件の賞賛
返信
1 解決策
2,007件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport

Yes it could be done using the LS1043. There isn't specific pins for your purpose so you can use the GIOP's or use the JTAG's pins.

Unfortunately we don't have any example of it.

  

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,008件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport

Yes it could be done using the LS1043. There isn't specific pins for your purpose so you can use the GIOP's or use the JTAG's pins.

Unfortunately we don't have any example of it.

  

0 件の賞賛
返信
1,963件の閲覧回数
AntoNico10
Contributor II
Thank you for the verifying!
0 件の賞賛
返信