External SRAM-like Bus Performance Limit due to Internal Bus Latency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External SRAM-like Bus Performance Limit due to Internal Bus Latency

1,292 Views
aivchenko
Contributor II

Does Layerscape architecture like LS1028A or LS1046A have the same limitations on the external parallel bus?

0 Kudos
Reply
1 Reply

1,227 Views
Pavel
NXP Employee
NXP Employee

The IFC controller is used for connection to NOR or SRAM memory.

This IFC controller supports burst size up to 256 bytes.

Usually qDMA is used for data transfers from memory to memory.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply