External SRAM-like Bus Performance Limit due to Internal Bus Latency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External SRAM-like Bus Performance Limit due to Internal Bus Latency

1,293件の閲覧回数
aivchenko
Contributor II

Does Layerscape architecture like LS1028A or LS1046A have the same limitations on the external parallel bus?

0 件の賞賛
返信
1 返信

1,228件の閲覧回数
Pavel
NXP Employee
NXP Employee

The IFC controller is used for connection to NOR or SRAM memory.

This IFC controller supports burst size up to 256 bytes.

Usually qDMA is used for data transfers from memory to memory.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信