Examples of Reset Configuration Word Source File ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Examples of Reset Configuration Word Source File ?

ソリューションへジャンプ
3,688件の閲覧回数
smiller2
Contributor IV

Are the Code Warrior files that generate the Reset Configuration Word available for the FRWY-LS1046A Board and the LS1046A Reference Design?     I am trying to construct the RCW for our design before layout.   My problem is I have no experience in either Code Warrior or generating these files, so I have no clue what is a normal setting versus stuff that I have screwed up.    If I had the files for the demo boards then at least I would have a starting point.   I searched the website, but could not find a download of these files. 

 

Thank you. 

0 件の賞賛
返信
1 解決策
3,660件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Sections 8.6 - 8.6.3 for RCW overriding using CodeWarrior in the ARMv8_Targeting_Manual.pdf file.

See also the Sections 8.4 -9.4.2.

元の投稿で解決策を見る

3 返答(返信)
3,681件の閲覧回数
Pavel
NXP Employee
NXP Employee

See attachment. This attachment contains RCW files for the FRWY-LS1046a board from NXP LSDK.

Use these files as RCW examples.

0 件の賞賛
返信
3,674件の閲覧回数
smiller2
Contributor IV

Thank you for the example files.   I downloaded them, but I do not know exactly how to get them into Code Warrior.    I tried following the steps in :

https://www.nxp.com/docs/en/user-guide/QCVS_PBL_User_Guide.pdf

 

I do file->New->QorIQ Configuration Project  and follow the steps.  I select that I want to import and point to one of the files from the zip file.   When I click "Finish"  no errors are reported.   However, no project folder is ever created either.    I tried both binary and text file.  

The Code Warrior version is:

Version: 11.5.2
Build Id: 210130

 

This is the free version.   However, from what I am told, that should be sufficient to at least generate a RCW file.    

Thanks.

 

0 件の賞賛
返信
3,661件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Sections 8.6 - 8.6.3 for RCW overriding using CodeWarrior in the ARMv8_Targeting_Manual.pdf file.

See also the Sections 8.4 -9.4.2.