Ethernet Errors Count on LS1046A-RDB board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet Errors Count on LS1046A-RDB board

ソリューションへジャンプ
2,392件の閲覧回数
JSKIM
Contributor III

I am working on a LS1046A-RDB board and LSDK2004 version. When I set ip address into ethernet interface, the ethernet error counter shows.

I found out the following error messages and error count.

what cause of that?

root@qemuarm64:~# ifconfig eth0 192.168.47.111
root@qemuarm64:~# [ 1467.724862] fsl_dpa: fsl-dpa: non-zero error counters in fman statistics (sysfs)
[ 1468.476559] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:9f:05:3d:0c
inet addr:192.168.47.111 Bcast:192.168.47.255 Mask:255.255.255.0
inet6 addr: fe80::204:9fff:fe05:3d0c/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:39 dropped:0 overruns:0 frame:0
TX packets:6 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:516 (516.0 B)
Memory:1ae4000-1ae4fff

root@qemuarm64:~#

0 件の賞賛
返信
1 解決策
2,359件の閲覧回数
JSKIM
Contributor III

Thank for your reply. 

I fixed the problem. i checked mac & phy layer, phy interface caused the issue.

i just wonder the difference between kernel device tree phy define info and system applied phy interface info. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,360件の閲覧回数
JSKIM
Contributor III

Thank for your reply. 

I fixed the problem. i checked mac & phy layer, phy interface caused the issue.

i just wonder the difference between kernel device tree phy define info and system applied phy interface info. 

0 件の賞賛
返信
2,377件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download bootpartition with the following command, and use Image and fsl-ls1046a-rdb-sdk.dtb provided in the bootpartition tar ball.

$ wget https://www.nxp.com/lgfiles/sdk/lsdk2004/bootpartition_LS_arm64_lts_5.4.tgz

 

How did you generate images with LSDK 2004?
How did you boot up the target board with the generated images? Would you please provide your whole boot up log on the target board?

0 件の賞賛
返信