Ethernet Driver for LS1021A?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet Driver for LS1021A?

3,546件の閲覧回数
sukruthrameshba
Contributor III

Hi,

 

We are using a custom made eval board in which LS1021A microprocessor is populated.

Hence Linux BSP , which NXP provides doesn't support this board.

Moreover, We are developing a very lean application on this board for which are not going with Linux platform.

 

Hence we are using Code Warrior IDE for development of our application.

It would be of great support if you can provide us , simple eth driver which can transmit and receive normal eth packet using any of the eTSEC controller? 

 

Regards,

Sukruth

ラベル(1)
タグ(1)
0 件の賞賛
返信
8 返答(返信)

3,301件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no low-level Ethernet example code.

It is possible to refer to the Ethernet driver in U-Boot.

0 件の賞賛
返信

3,301件の閲覧回数
sukruthrameshba
Contributor III

Can you please attach the Ethernet driver in U-Boot?

As i currently do not have those files.

0 件の賞賛
返信

3,301件の閲覧回数
ufedor
NXP Employee
NXP Employee

U-Boot sources could be obtained here:

sdk/u-boot.git - Freescale PowerPC u-boot Tree 

0 件の賞賛
返信

3,301件の閲覧回数
sukruthrameshba
Contributor III

Thank you!

Got the reference code.

But the heading says , Freescale PowerPC u-boot Tree.

Is it the same for Layerscape arichitecture LS1021A processor?

0 件の賞賛
返信

3,301件の閲覧回数
ufedor
NXP Employee
NXP Employee

The eTSEC IP is the same (as on P1 family), so the code is compatible.

0 件の賞賛
返信

3,301件の閲覧回数
sukruthrameshba
Contributor III

Okay….Thanks☺

0 件の賞賛
返信

3,301件の閲覧回数
sukruthrameshba
Contributor III

Sorry, I could not locate Ethernet driver file in the below link.

Can you please attach the relevant Ethernet driver file for reference?

0 件の賞賛
返信

3,301件の閲覧回数
ufedor
NXP Employee
NXP Employee
0 件の賞賛
返信