Error F001 EmuVariableRuntimeDxe.inf NOT found in DSC file while compiling sd card uefi boot using LSDK 18.09 or older bootflow with ppa on LS1046ARDB.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error F001 EmuVariableRuntimeDxe.inf NOT found in DSC file while compiling sd card uefi boot using LSDK 18.09 or older bootflow with ppa on LS1046ARDB.

跳至解决方案
6,894 次查看
kg8herve
Contributor II

Hi everyone,

For some reason I need to deploy uefi/edk2 on LS1046ARDB using LSDK 18.09 or older ppa bootflow. I've Tried to compile  edk2 for sd card boot  this way:

Get the edk2:

git clone https://source.codeaurora.org/external/qoriq/qoriq-components/uefi

git checkout LS1046ARDB-QUEFI_DASH_V5-0_1806

Get the edk2-platforms:

git clone https://source.codeaurora.org/external/qoriq/qoriq-components/edk2-platforms

Compilation:

export PATH=gcc-linaro-4.9-2016.02-x86_64_aarch64-linux-gnu/bin:$PATH

export ARCH=arm64

export CROSS_COMPILE=aarch64-linux-gnu-

source edksetup.sh

cd LS1046aRdbPkg

source  ls1046a_env.cshrc

cd ../

make -C BaseTools/Source/C

cd LS1046aRdbPkg

./build.sh RELEASE SD ./path_to_uboot/tools

After execution of above steps, i get this log output:

..........................................
Welcome to LS1046A UEFI Build environment
..........................................
Compiling for RELEASE boot
Using mkimage utility is available at this path: uboot/tools/
(Hint: Usually this is the absolute path of the u-boot/tools directory)
Initializing workspace
Loading previous configuration from uefi/Conf/BuildEnv.sh
WORKSPACE: ./uefi
EDK_TOOLS_PATH: uefi/BaseTools
CONF_PATH: uefi/Conf
Build environment: Linux-4.15.0-99-generic-x86_64-with-Ubuntu-18.04-bionic
Build start time: 19:29:16, May.15 2020

WORKSPACE        = uefi
PACKAGES_PATH    = uefi/edk2-platforms
ECP_SOURCE       = uefi/EdkCompatibilityPkg
EDK_SOURCE       = uefi/EdkCompatibilityPkg
EFI_SOURCE       = uefi/EdkCompatibilityPkg
EDK_TOOLS_PATH   = uefi/BaseTools
CONF_PATH        = uefi/Conf


Architecture(s)  = AARCH64
Build target     = RELEASE
Toolchain        = GCC49

Active Platform          = uefi/LS1046aRdbPkg/LS1046aRdbPkgNonXipBoot.dsc
Flash Image Definition   = uefi/LS1046aRdbPkg/LS1046aRdbPkgNonXipBoot.fdf

Processing meta-data .

build.py...
 : error F001: Module uefi/MdeModulePkg/Universal/Variable/EmuRuntimeDxe/EmuVariableRuntimeDxe.inf NOT found in DSC file; Is it really a binary module?
    
 

- Failed -
Build end time: 19:29:17, May.15 2020
Build total time: 00:00:01

How can i resolve this problem?

Thanks in advance.

1 解答
6,758 次查看
yipingwang
NXP TechSupport
NXP TechSupport

SD UEFI image for LS1046ARDB is not supported, only QSPI UEFI image is supported.

Please refer to the following QSPI UEFI flash.

$ cd uefi
$ source edksetup.sh
$ cd LS1046aRdbPkg
$ source ls1046a_env.cshrc
$ cd ../BaseTools
$ make clean
$ make

$ cd ../LS1046aRdbPkg
$./build.sh RELEASE QSPI clean
$./build.sh RELEASE QSPI

UEFI Firmware Image:
uefi/Build/LS1046aRdb/RELEASE_GCC49/FV/LS1046ARDB_EFI.fd
UEFI Non Volatile Variables Image:
uefi/Build/LS1046aRdb/RELEASE_GCC49/FV/LS1046ARDBNV_EFI.fd

在原帖中查看解决方案

5 回复数
6,404 次查看
AnjanaR-PS
Contributor I

Is SD UEFI supported for LS1046AFRWY, LS1046ARDB and LX2160ARDB in latest LSDK (20.12) ?

0 项奖励
回复
6,759 次查看
yipingwang
NXP TechSupport
NXP TechSupport

SD UEFI image for LS1046ARDB is not supported, only QSPI UEFI image is supported.

Please refer to the following QSPI UEFI flash.

$ cd uefi
$ source edksetup.sh
$ cd LS1046aRdbPkg
$ source ls1046a_env.cshrc
$ cd ../BaseTools
$ make clean
$ make

$ cd ../LS1046aRdbPkg
$./build.sh RELEASE QSPI clean
$./build.sh RELEASE QSPI

UEFI Firmware Image:
uefi/Build/LS1046aRdb/RELEASE_GCC49/FV/LS1046ARDB_EFI.fd
UEFI Non Volatile Variables Image:
uefi/Build/LS1046aRdb/RELEASE_GCC49/FV/LS1046ARDBNV_EFI.fd

6,758 次查看
kg8herve
Contributor II

Thanks for your answer. I have one  more question for clarification:

Is your answer also valid when using uefi with tfa boot flow (LSDK 19.09) with SD Card on LS1046ARDB?

When trying that, uefi start booting then i get this error :

Firmware Volume for Variable Store is corrupted

ASSERT_EFI_ERROR (Status = Volume Corrupt)

VariableDxe.c(479): !EFI_ERROR (Status)
0 项奖励
回复
6,758 次查看
yipingwang
NXP TechSupport
NXP TechSupport

SD UEFI  for LS1046ARDB is not supported either in LSDK 19.09.

6,758 次查看
kg8herve
Contributor II

Thank for your reply.

0 项奖励
回复