Enabling the Ethernet Switch on LS1028ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling the Ethernet Switch on LS1028ARDB

1,548 Views
sebastian_plama
Contributor II

I am trying to follow this documentation to enable the Switch on the LS1028ARDB:

https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-558A9D18-5FA4-4E88-B...

All mentioned commands fail with the same error message:

 

 

 

root@localhost:~# restool dpsw create --num-ifs=5 --max-vlans=16 --max-fdbs=1 --options="DPSW_OPT_CTRL_IF_DIS"
error: Did not find a device file

 

 

 


The documentation also contains this line:

The following section describes the main commands to create a switch starting from the dpl-eth.0x2A_0x41.dtb DPL file.

Is there any description what this file is, where to find it, how to use it?

0 Kudos
Reply
2 Replies

1,536 Views
sebastian_plama
Contributor II

Thanks, I will try this.

Is there any way to know which parts of this very long document are relevant for which boards?

0 Kudos
Reply

1,542 Views
bpe
NXP Employee
NXP Employee

restool and DPL files are valid only for devices equipped with DPAA2. LS1028A does not have it. Study this section of LSDK online documentation on how to work with LS1028A on-chip switch.

 

Hope this helps

Platon

 

0 Kudos
Reply