Enabling forward traffic on switch ports from DPSW (DPAA2) without running OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling forward traffic on switch ports from DPSW (DPAA2) without running OS

Jump to solution
2,599 Views
rgallais
Contributor I

Dear Community,

From my trials, it seems that applying DPL from U-Boot is not enough to enable the DPSW and enable forwarding traffic on switch ports from DPSW and I needed to run the following command "ip link set eth<N> master <brX>" (under Linux) to do it.

Is there a way to enable forward traffic on switch ports from DPSW (DPAA2) without running OS ?

It would be great to do so from DPL configuration but I haven't found how to do it from LSDK UG document.

Regards,

 

0 Kudos
Reply
1 Solution
2,585 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please get mc_utils source code folder in flexbuild_lsdk2108/components/firmware/mc_utils/.

Please refer to dpl file in mc_utils/config/ls2088a/LS2088A-RDB/custom/dpl-eth-dpsw.0x2A_0x41.dts.

/* ------------ DPSW ---------------*/
obj@900 {
obj_name = "dpsw@0";
};

...

objects {

...
/* ------------ DPSW ---------------*/
dpsw@0 {
compatible = "fsl,dpsw";
options = "DPSW_OPT_CTRL_IF_DIS";
max_vlans = <0x10>;
max_fdbs = <0x1>;
num_fdb_entries = <0x400>;
fdb_aging_time = <0x12c>;
num_ifs = <0x4>;
max_fdb_mc_groups = <0x40>;
};

}

connections {
connection@0{
/* Copper port (ETH0 on the RDB chassis) */
endpoint1 = "dpni@0";
endpoint2 = "dpmac@5";
};

connection@1 {
/* Copper port (ETH1 on the RDB chassis) */
endpoint1 = "dpsw@0/if@0";
endpoint2 = "dpmac@6";
};

connection@2 {
/* Copper port (ETH2 on the RDB chassis) */
endpoint1 = "dpsw@0/if@1";
endpoint2 = "dpmac@7";
};

connection@3 {
/* Copper port (ETH3 on the RDB chassis) */
endpoint1 = "dpsw@0/if@2";
endpoint2 = "dpmac@8";
};

connection@4 {
/* Internal port (ni1 in Linux) */
endpoint1 = "dpsw@0/if@3";
endpoint2 = "dpni@1";

};
};

View solution in original post

2 Replies
2,583 Views
rgallais
Contributor I

Thank you for your inputs ! I succeeded to deploy the DPSW with forward traffic enabled under U-Boot without running Linux.

Regards,

0 Kudos
Reply
2,586 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please get mc_utils source code folder in flexbuild_lsdk2108/components/firmware/mc_utils/.

Please refer to dpl file in mc_utils/config/ls2088a/LS2088A-RDB/custom/dpl-eth-dpsw.0x2A_0x41.dts.

/* ------------ DPSW ---------------*/
obj@900 {
obj_name = "dpsw@0";
};

...

objects {

...
/* ------------ DPSW ---------------*/
dpsw@0 {
compatible = "fsl,dpsw";
options = "DPSW_OPT_CTRL_IF_DIS";
max_vlans = <0x10>;
max_fdbs = <0x1>;
num_fdb_entries = <0x400>;
fdb_aging_time = <0x12c>;
num_ifs = <0x4>;
max_fdb_mc_groups = <0x40>;
};

}

connections {
connection@0{
/* Copper port (ETH0 on the RDB chassis) */
endpoint1 = "dpni@0";
endpoint2 = "dpmac@5";
};

connection@1 {
/* Copper port (ETH1 on the RDB chassis) */
endpoint1 = "dpsw@0/if@0";
endpoint2 = "dpmac@6";
};

connection@2 {
/* Copper port (ETH2 on the RDB chassis) */
endpoint1 = "dpsw@0/if@1";
endpoint2 = "dpmac@7";
};

connection@3 {
/* Copper port (ETH3 on the RDB chassis) */
endpoint1 = "dpsw@0/if@2";
endpoint2 = "dpmac@8";
};

connection@4 {
/* Internal port (ni1 in Linux) */
endpoint1 = "dpsw@0/if@3";
endpoint2 = "dpni@1";

};
};