eMMC and LS1046a hardware design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMMC and LS1046a hardware design

2,156 次查看
Ellu24
Contributor III

Hello

I am doing a new hardware design using ls1046a and now trying to interface eMMC. I have some doubts regarding this.

1) I am planning to use emmc version 5.1 and whether it is supported by  processor or not.

2) to which pin of the processor hardware reset and RCLK of the emmc should connect.

0 项奖励
回复
3 回复数

2,128 次查看
yipingwang
NXP TechSupport
NXP TechSupport

1. Please take a look at sections 19.1.1 and 19.1.2 of the LS1046A Ref Manual, these list  features and protocols supported by the processor. It can work with eMMC 5.1 devices, but supports only eMMC 4.5 features.

2. Please refer to https://www.nxp.com.cn/docs/en/application-note/AN5252.pdf

0 项奖励
回复

2,125 次查看
Ellu24
Contributor III

Thanks for the reply. can you please suggest me, where to connect the hardware reset of eMMC.

0 项奖励
回复

2,084 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "5.6.1 eSDHC pin termination recommendations" in AN5252.pdf.

0 项奖励
回复