Enabling Cryptographic Hardware Acceleration on LS1088ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling Cryptographic Hardware Acceleration on LS1088ARDB

1,275件の閲覧回数
reza_m
Contributor II

What kernel modules do I need to install to get the LS1088ARDB to see the ARM crypto drivers. I am running layerscape 18.06 and using openwrt 19.07

1 返信

1,226件の閲覧回数
bpe
NXP Employee
NXP Employee

ARM cryptographic support code is located under /arch/arm64/crypto/. You can look
at Kconfig and Makefile in that directory to see what options to enable to build
the necessary modules.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------