ECC keys for Secure Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ECC keys for Secure Boot

跳至解决方案
3,366 次查看
nb1
Contributor I

Hi,

I'm trying to determine whether or not ECC keys are supported in ISBC, as Super Root Keys (SRKs).

The Trust Arch User Guide vaguely mentions "RSA or ECC private keys" for signing, but any other descriptions (including the LSDK User Guide), pictures or examples I've seen very specifically and exclusively refer to RSA keys up to 4K.

I'd appreciate if you could let me know whether ECC keys are supported, and if so, the supported curves please. If you could point me to some documentation that would be great as well.

Thank you!

0 项奖励
回复
1 解答
3,351 次查看
bpe
NXP Employee
NXP Employee

ISBC supports only RSA. CST has no valid input file options for ECC in ISBC
headers. Only in the ESBC you have an option to use the ARM CoT for selecting
x509 format for ECC key or RSA key.

Best Regards,
Platon

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,352 次查看
bpe
NXP Employee
NXP Employee

ISBC supports only RSA. CST has no valid input file options for ECC in ISBC
headers. Only in the ESBC you have an option to use the ARM CoT for selecting
x509 format for ECC key or RSA key.

Best Regards,
Platon

 

 

0 项奖励
回复
3,343 次查看
nb1
Contributor I

Thank you!

0 项奖励
回复