Hi,
As I know, LS1046 platform has ASK SDK(as below link) to combine DPDK and strongswan to support complete Ikev2 feature
May I know on DPAA2 platform (LX2160 or LX2080) also has the same solutoin?
Thank you.
Jack Ho
Hi @jackho,
In the following link you will find information related to StrongSwan and Ikev2 on the LX2160
https://www.nxp.com/webapp/Download?colCode=LX2160ASFSIBPB
Due to is not available an ASK for LX2160 instead of that you can use the ASF (Application Specific Fastpath)
Regards,
Sebastian
Hi @SebastianG,
Thank you for your detail information.
Does this solution also work with DPDK? it seems that mentions this in this document.
Regards,
Jack Ho
HI @SebastianG
Sorry, I saw it mentions about DPDK.
It seems a good solution.
Also, I saw that NXP maintains VPP package, It seems the Network protocol layer is VPP(supports IKEv2) and Network I/O is DPDK, Do you think this may also be a solution?
Do you
Thanks
Jack Ho
Hi Jackho, I am also trying to get StrongSwan to work with DPDK but on the LS1046A. It is not obvious if a special StongSwan plugin is needed for this. I could not find mention of StrongSwan in the ASK SDK docs only than it supports IKEv2. Note I am not using the ASK rather the LayerScape SDK. If I find out anything further I will note it here.