Does DPDK support IPSEC with Ikev2 and storongswan on DPAA2 platform?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does DPDK support IPSEC with Ikev2 and storongswan on DPAA2 platform?

1,390 Views
jackho
Contributor III

Hi,

As I know, LS1046 platform has ASK SDK(as below link) to combine DPDK and strongswan to support complete Ikev2 feature

https://www.nxp.com/support/support/nxp-engineering-services/gateway-ask/layerscape-1046a-processor-...

May I know on DPAA2 platform (LX2160 or LX2080) also has the same solutoin?

Thank you.

Jack Ho

Tags (1)
0 Kudos
7 Replies

1,334 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @jackho,

In the following link you will find information related to StrongSwan and Ikev2 on the LX2160

https://www.nxp.com/webapp/Download?colCode=LX2160ASFSIBPB

Due to is not available an ASK for LX2160 instead of that you can use the ASF (Application Specific Fastpath)

Regards,

Sebastian

0 Kudos

1,281 Views
jackho
Contributor III

Hi @SebastianG,

Thank you for your detail information.

Does this solution also work with DPDK? it seems that mentions this in this document.

Regards,

Jack Ho

0 Kudos

1,240 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @jackho,

Yes, this solution work with DPDK

Regards,

Sebastian

0 Kudos

1,278 Views
jackho
Contributor III

HI @SebastianG 

Sorry, I saw it mentions about DPDK.

It seems a good solution.

Also, I saw that NXP maintains VPP package, It seems the Network protocol layer is VPP(supports IKEv2) and Network I/O is DPDK, Do you think this may also be a solution?

Do you  

Thanks

Jack Ho

0 Kudos

1,238 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @jackho,

Yes is a good solution due to the fact that the VPP supports IKEv2

Regards,

Sebastian

0 Kudos

1,350 Views
IanHailey
Contributor II

Hi Jackho, I am also trying to get StrongSwan to work with DPDK but on the LS1046A. It is not obvious if a special StongSwan plugin is needed for this. I could not find mention of StrongSwan in the ASK SDK docs only than it supports IKEv2. Note I am not using the ASK rather the LayerScape SDK. If I find out anything further I will note it here.

0 Kudos

888 Views
hemantagrawal
NXP Employee
NXP Employee
0 Kudos