Discrepancy Between LS1043A Datasheet and Design Guide

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Discrepancy Between LS1043A Datasheet and Design Guide

1,581件の閲覧回数
abhinav
Contributor I

Hi,

I have a question pertaining to the LS1043A and LS10xxA family. The datasheet of this device lists +/-30mV as the recommended value for the rail on VDD. The design guide for supply filtering, however, lists the requirements as +50mV/-30mV. This is a significant difference at this tight of a spec so I was posting for clarification on which of these is correct, and whether the datasheet is referring solely to DC variation and does not include transients or not.

Thanks,

Abhinav.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,483件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

For positive transient response, it must be below Vdd + 50 mV (although it may exceed Vdd + 30 mV)
For negative transient response, it must be within Vdd - 30 mV.

The +50mv -30mv is total deviation due to thermal, di/dt of transients, base regulation and ripple from the regulator.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信