Device Tree Configuration Error: Device Tree Value Out of Range for 32-Bit Array Element

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Tree Configuration Error: Device Tree Value Out of Range for 32-Bit Array Element

7,350件の閲覧回数
csr202
Contributor II

I am attempting to configure memory-mapped regions for the NOR Flash and FRAM devices.

NOR Flash - 256MB window for XSPI1_A, CS0
Start address: 0x000020000000h
End address: 0x00002FFFFFFFh

NOR Flash - 256MB window for XSPI1_A, CS1
Start address: 0x000400000000h
End address: 0x00040FFFFFFFh

FRAM - 512KB window for XSPI1_B, CS1
Start address: 0x000410000000h
End address: 0x00041FFFFFFFh

I have configured the DTS (Device Tree Source) "reg" property for the flash and FRAM regions. However, during the DTB (Device Tree Blob) compilation, I encounter the following error:

"Device tree value out of range for 32-bit array element." This error occurs due to the use of 64-bit addresses in the "reg" property.

Could you please advise on how to configure a 64-bit address with the "reg" property in the device tree?

Device Tree Configuration:

```device-tree
&fspi {
status = "okay";
#address-cells = <2>;
#size-cells = <1>;

/* Memory-mapped regions for the Flash and FRAM devices */
reg = <0x0 0x20000000 0x0 0x10000000>, /* Flash region 1: 256MB */
<0x0 0x400000000 0x0 0x10000000>, /* Flash region 2: 256MB */
<0x0 0x410000000 0x0 0x80000>; /* FRAM region: 512KB */

flash@0 {
compatible = "jedec,spi-nor";
spi-max-frequency = <90000000>;
reg = <0x0 0x20000000 0x0 0x10000000>;
spi-rx-bus-width = <4>;
spi-tx-bus-width = <4>;
};

flash@1 {
compatible = "jedec,spi-nor";
spi-max-frequency = <90000000>;
reg = <0x0 0x400000000 0x0 0x10000000>;
spi-rx-bus-width = <4>;
spi-tx-bus-width = <4>;
};

fram@3 {
compatible = "jedec,spi-nor";
spi-max-frequency = <50000000>;
reg = <0x0 0x410000000 0x0 0x80000>;
spi-rx-bus-width = <4>;
spi-tx-bus-width = <4>;
};
};
```

0 件の賞賛
返信
10 返答(返信)

6,329件の閲覧回数
csr202
Contributor II

any update ?

0 件の賞賛
返信

6,365件の閲覧回数
csr202
Contributor II

@yipingwang I tried configuring reg property for FlexSPI Region #2 in device tree as below.

reg = <0x00 0x20c0000 0x00 0x10000>,

<0x04 0x10000000 0x00 0x00080000>; //512KB

I could see memory region listed in /proc/iomem after adding following code in the kenrel "drivers/spi/spi-nxp-fspi.c"

----------------------------------------------------

res = platform_get_resource_byname(pdev, IORESOURCE_MEM, "fspi_mmap");

...

+ if (!devm_request_mem_region(dev, res->start, resource_size(res),res->name)) {
+ dev_err(dev, "fspi can't request region for resource %pR\n", res);
+ ret = -EBUSY;
+ goto err_put_ctrl;
+ }

----------------------------------------------------

$cat /proc/iomem 
....
020c0000-020cffff : 20c0000.spi fspi_base

410000000-41007ffff : fspi_mmap
....
Question:

I could use ioremap in a custom driver to map physical memory at base address 0x410000000.

However, when I get the kernel panic when I try to use the virtual address (from ioremap).

[ 636.001611] Internal error: synchronous external abort: 96000210 [#1] PREEMPT SMP 

Am I missing any configuration here? Does nxp-fspi driver supports memory mapped access of FlexSPI Region #2 from below system memory map ? 

System memory map

0x0000_2000_0000        0x0000_2FFF_FFFF       256MB   FlexSPI Region #1
0x0004_0000_0000        0x0004_0FFF_FFFF       256MB   SPI Hole                                            
Collapsed away by remapping logic to merge FlexSPI Region #1
0x0004_1000_0000        0x0004_FFFF_FFFF       3.75GB   FlexSPI Region #2(256MB-4GB)  3.75GB

0 件の賞賛
返信

6,348件の閲覧回数
csr202
Contributor II
@yipingwang any update on this thread?
0 件の賞賛
返信

7,286件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to fsl-lx2160a-rdb.dts for how to define fspi devices. No need to define memory mapped region.

&fspi {
status = "okay";

mt35xu512aba0: flash@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "spansion,m25p80";
m25p,fast-read;
spi-max-frequency = <50000000>;
reg = <0>;
spi-rx-bus-width = <8>;
spi-tx-bus-width = <8>;
};

mt35xu512aba1: flash@1 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "spansion,m25p80";
m25p,fast-read;
spi-max-frequency = <50000000>;
reg = <1>;
spi-rx-bus-width = <8>;
spi-tx-bus-width = <8>;
};
};

0 件の賞賛
返信

7,267件の閲覧回数
csr202
Contributor II
I have successfully configured the fspi nor flash device tree node with partitions and accessed it as mtd partitions from Linux. I could also access the fram mtd partitions after adding the jedec id for fram in the spi-nor driver.

I am interested in accessing the fram memory-mapped regions from Linux using ioremap. Could you please provide guidance on how to configure it in the device tree so that it can be accessed from the Linux system memory?
0 件の賞賛
返信

7,244件の閲覧回数
csr202
Contributor II
Any update on this thread?
0 件の賞賛
返信

7,235件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

System memory map

  • 0x0000_2000_0000        0x0000_2FFF_FFFF       256MB   FlexSPI Region #1
  • 0x0004_0000_0000        0x0004_0FFF_FFFF       256MB   SPI Hole                                             Collapsed away by remapping logic to merge FlexSPI Region #1
  • 0x0004_1000_0000        0x0004_FFFF_FFFF       3.75GB   FlexSPI Region #2(256MB-4GB)  3.75GB

CCSR Block address map

        0x20C_0000 -      0x20C_FFFF QSPI (Flex SPI)

Please refer to fsl-lx2160a.dtsi

fspi: spi@20c0000 {
compatible = "nxp,lx2160a-fspi";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x0 0x20c0000 0x0 0x10000>,
<0x0 0x20000000 0x0 0x10000000>;
reg-names = "fspi_base", "fspi_mmap";
interrupts = <GIC_SPI 25 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clockgen 4 3>, <&clockgen 4 3>;
clock-names = "fspi_en", "fspi";
status = "disabled";
};

You could define reg device node as the following.

reg = <0x0 0x20c0000 0x0 0x10000>,

<0x4 0x10000000 0x0 0x30000000>;

You could refer to Documentation/devicetree/bindings/spi/spi-nxp-fspi.txt for details.

0 件の賞賛
返信

7,211件の閲覧回数
csr202
Contributor II

Thanks @yipingwang 

I could configure reg property for FlexSPI Region #2 in device tree as you suggested below.

reg = <0x00 0x20c0000 0x00 0x10000>,

<0x04 0x10000000 0x00 0x30000000>;

However, I don't see this memory-mapped region listed in  /proc/iomem.

I'm trying to access this memory-mapped region (physical address) and use ioremap to map it into the kernel's virtual address space and then read from or write to it using ioread and iowrite functions.

Is there any additional configuration needed in device tree for this?

I'm using below dts configuration, 

spi@20c0000 {
compatible = "nxp,lx2160a-fspi";
#address-cells = <0x01>;
#size-cells = <0x00>;
reg = <0x00 0x20c0000 0x00 0x10000 0x04 0x10000000 0x00 0x30000000>;
reg-names = "fspi_base\0fspi_mmap";
 
flash@0 {
compatible = "jedec,spi-nor";
reg = <0x00>;
....
}
flash@1 {
compatible = "jedec,spi-nor";
reg = <0x01>;
};
 
fram@3 {
compatible = "jedec,spi-nor";
reg = <0x03>;
};

 

0 件の賞賛
返信

7,132件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could refer to nxp_fspi_read_ahb function in drivers/spi/spi-nxp-fspi.c.

static int nxp_fspi_read_ahb(struct nxp_fspi *f, const struct spi_mem_op *op)
{
u32 start = op->addr.val;
u32 len = op->data.nbytes;

/* if necessary, ioremap before AHB read */
if ((!f->ahb_addr) || start < f->memmap_start ||
start + len > f->memmap_start + f->memmap_len) {
if (f->ahb_addr)
iounmap(f->ahb_addr);

f->memmap_start = start;
f->memmap_len = len > NXP_FSPI_MIN_IOMAP ?
len : NXP_FSPI_MIN_IOMAP;

f->ahb_addr = ioremap_wc(f->memmap_phy + f->memmap_start,
f->memmap_len);

if (!f->ahb_addr) {
dev_err(f->dev, "failed to alloc memory\n");
return -ENOMEM;
}
}

/* Read out the data directly from the AHB buffer. */
memcpy_fromio(op->data.buf.in,
f->ahb_addr + start - f->memmap_start, len);

return 0;
}

0 件の賞賛
返信

7,155件の閲覧回数
csr202
Contributor II

@yipingwang Whenever you have the opportunity, please share your thoughts on this.

0 件の賞賛
返信