Design guidelines/files for LS102MA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Design guidelines/files for LS102MA

1,848 Views
chq
Contributor I

Hi,

Is there a design guideline for LS102MA and the LS102X series? Also where can I download/find the design files for the reference design?

Thank you very much.

Labels (1)
0 Kudos
Reply
1 Reply

1,706 Views
andrei_skok
NXP Employee
NXP Employee

Design guidelines for LS102MA and the LS1021A processors can be found at the following links:

QorIQ LS1024A - Data Sheet

https://www.freescale.com/webapp/Download?colCode=LS1024A

AN5010, QorIQ LS1024A Family Design Checklist

https://www.freescale.com/webapp/Download?colCode=AN5010

LS1021A, QorIQ LS1021A Data Sheet

https://www.freescale.com/webapp/Download?colCode=LS1021A

AN4878, QorIQ LS1021A Design Checklist

http://cache.freescale.com/files/32bit/doc/app_note/AN4878.pdf

AN5097, Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces

http://cache.freescale.com/files/32bit/doc/app_note/AN5097.pdf

All publicly available documentation for the LS1024A and LS1021A reference designs can be found at the following links:

http://www.freescale.com/products/arm-processors/qoriq-arm-processors/qoriq-ls1024a-reference-design...?

http://www.freescale.com/products/arm-processors/qoriq-arm-processors/ls1021a-iot-gateway-reference-...?

All design files for these boards are Freescale Confidential Proprietary and can only be provided under non-disclosure agreement (NDA).  Please create a Service request on our WEB site and ask the Freescale employee who signed an NDA with your company to send Freescale technical support an e-mail confirming that an active NDA exists with your company that covers the requested information.  After an e-mail confirmation is received, Freescale technical support will attempt to locate and provide the requested information.

Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply