Data Path Routing on LS1021A-IOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Data Path Routing on LS1021A-IOT

1,437 Views
anilsharma
Contributor I

Hi,

We have requirement for data path routing in LS1021A-IOT board. Does it supports

    • DPAA offloading
    • FMAN/QMan/BMan
    • Application Specific Fast Path

In SDK documentation these feature are not applicable for IOT board. Could someone tell how to enable them on LS1021A-iot?

Regards,

Anil

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,276 Views
bpe
NXP Employee
NXP Employee

LS1021A is not equipped with DPAA, therefore, none of DPAA components,

such as QMAN, FMAN, BMAN or RMAN is available in this processor.

LS1021A Ethernet controllers, eTSECs, however, are equipped with a frame

parser/filer (see LS1021ARM, Section 20.9.4) which allows ASF to be

supported on your  device. Refer to your board SDK documentation for

more details:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/qoriq-arm-processors/qori...


Have a great day

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply