Data Path Routing on LS1021A-IOT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Data Path Routing on LS1021A-IOT

1,449 次查看
anilsharma
Contributor I

Hi,

We have requirement for data path routing in LS1021A-IOT board. Does it supports

    • DPAA offloading
    • FMAN/QMan/BMan
    • Application Specific Fast Path

In SDK documentation these feature are not applicable for IOT board. Could someone tell how to enable them on LS1021A-iot?

Regards,

Anil

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,288 次查看
bpe
NXP Employee
NXP Employee

LS1021A is not equipped with DPAA, therefore, none of DPAA components,

such as QMAN, FMAN, BMAN or RMAN is available in this processor.

LS1021A Ethernet controllers, eTSECs, however, are equipped with a frame

parser/filer (see LS1021ARM, Section 20.9.4) which allows ASF to be

supported on your  device. Refer to your board SDK documentation for

more details:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/qoriq-arm-processors/qori...


Have a great day

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复