DSR eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSR eMMC

Jump to solution
2,919 Views
christiansielaf
Contributor III

Hi all,

how we can adjust the driver strength of the I/O's for the eMMC (eSDHC) controller? We are working on a coustomer LS1021A design, with really short traces between eMMC and processor. We could observ overshoot at the CMD line which are out of operation range.

 

We realy appreciate your response.

 

Best regards and thank you in advance,

Christian

Labels (1)
0 Kudos
Reply
1 Solution
2,716 Views
alexander_yakov
NXP Employee
NXP Employee

The fact that you are observing overshot means output driver strength needs to be reduced - output driver impedance is to low and needs to be increased. 

The typical way to increase output driver impedance is to place series resistor at the near (source) end of trace.

Output driving strength on eSDHC signals can not be changed by software.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,717 Views
alexander_yakov
NXP Employee
NXP Employee

The fact that you are observing overshot means output driver strength needs to be reduced - output driver impedance is to low and needs to be increased. 

The typical way to increase output driver impedance is to place series resistor at the near (source) end of trace.

Output driving strength on eSDHC signals can not be changed by software.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------