DRAM bus speed optimization test ls1021a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DRAM bus speed optimization test ls1021a

1,524 Views
winstonjacob
Contributor IV

I am using LS1021atwr board, here I need to do the DRAM bus speed optimization, please support me to do this test in LS1021atwr EVK board.

 

Regards

Winston

0 Kudos
Reply
3 Replies

1,518 Views
Bulat
NXP Employee
NXP Employee

Please clarify what means "DRAM bus speed optimization"?

Why do you think the DRAM bus speed is not optimized?

 

Regards

Bulat

 

0 Kudos
Reply

1,506 Views
winstonjacob
Contributor IV

Thanks for your reply @Bulat 

Please clarify what means "DRAM bus speed optimization"?

      I need to test the DRAM in various frequencies and various speed, is their any procedure available for this.

 

Regards

Winston

0 Kudos
Reply

1,490 Views
Bulat
NXP Employee
NXP Employee

Default DDR speed of the LS1021ATWR is 1600MT/s, this is a maximum possible speed for the LS1021A DDR controller. U-boot software provides setup for this speed.

If maximum possible speed is not "optimal" for you, you can test other speeds using DDR Validation tool, that is a part of QCVS. Note that DDR speed is defined by RCW, so for each DDR bus speed you will need to change RCW with desired MEM_PLL_RAT ratio. The tool will help with timing parameters for chosen bus frequency.

Regards,

Bulat

 

0 Kudos
Reply