DRAM ODT configruration value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DRAM ODT configruration value

1,289 Views
pb3
Contributor II

Hi, we've been working on our custom board based on LS1028A, the memory that we're using is IS43QR85120B-083RBLI in 512Mb x8 config - 2GB total.

We've managed to perform validation and so on, DDR seems to be working fine. 

We've performed some other tests like:

- enabled built self test in TF-A

- mtest in u-boot

- overnight tests on couple boards using memtester in Linux

Every test passed without any problems, however our electronic team is a bit worried about hardware level tests - from what they told me, the signal integrity does not match the requirements enforced by JEDEC. It's not a big gap between what JEDEC expects and what we have but still - it exists.

So my question is - what value in DDR controller determines the value that is being set in DRAM MR1 RTT_NOM? 

We've been using STATIC_DDR configuration you can see below:

+const struct ddr_cfg_regs static_1600 = {
+	.cs[0].bnds = 0x7F,
+	.cs[0].config = 0x80010322,
+	.timing_cfg[0] = 0x80550018,
+	.timing_cfg[1] = 0xBDB48F42,
+	.timing_cfg[2] = 0x0048D114,
+	.timing_cfg[3] = 0x010C1000,
+	.timing_cfg[4] = 0x01,
+	.timing_cfg[5] = 0x03401400,
+	.timing_cfg[7] = 0x13300000,
+	.timing_cfg[8] = 0x02115600,
+	.sdram_cfg[0] = 0x650C0004,
+	.sdram_cfg[1] = 0x00401010,
+	.dq_map[0] = 0x56C5AC2C,
+	.dq_map[1] = 0xAD6B0000,
+	.dq_map[2] = 0x00,
+	.dq_map[3] = 0x01600000,
+	.sdram_mode[0] = 0x01010610,
+	.sdram_mode[1] = 0x00,
+	.sdram_mode[2] = 0x00,
+	.sdram_mode[3] = 0x00,
+	.sdram_mode[4] = 0x00,
+	.sdram_mode[5] = 0x00,
+	.sdram_mode[6] = 0x00,
+	.sdram_mode[7] = 0x00,
+	.sdram_mode[8] = 0x0400,
+	.sdram_mode[9] = 0x04A40000,
+	.sdram_mode[10] = 0x00,
+	.sdram_mode[11] = 0x00,
+	.sdram_mode[12] = 0x00,
+	.sdram_mode[13] = 0x00,
+	.sdram_mode[14] = 0x00,
+	.sdram_mode[15] = 0x00,
+	.md_cntl = 0x00,
+	.interval = 0x18600618,
+	.data_init = 0xDEADBEEF,
+	.clk_cntl = 0x01C00000,
+	.init_addr = 0x00,
+	.ddr_sr_cntr = 0x0,
+	.init_ext_addr = 0x00,
+	.zq_cntl = 0x8A090705,
+	.wrlvl_cntl[0] = 0x86750604,
+	.wrlvl_cntl[1] = 0x05060700,
+	.wrlvl_cntl[2] = 0x08,
+	.cdr[0] = 0x80080000,
+	.cdr[1] = 0xA180,
+	.debug[28] = 0x01080F70
+};

 

The validation steps selects the following:

1) Read ODT and driver: 

  - ODT 60ohm / DRAM driver strength 34 ohm - full

2) Write ODT and driver

 - Controller DRV Strength - full strength / DRAM ODT - 60 ohm

As far as I understand, in the context of DRAM's MR1 RTT_NOM we're talking about 2) "Write ODT and driver" which was set during validation to 60 ohm, but I'm having difficulties understanding how the SDRAM_MODE register content reflects the RTT_NOM setting. 

I mean - how can I be sure that DRAM ODT 60ohm selected by validation was in fact programmed in DRAM? 

 

 

0 Kudos
Reply
1 Reply

1,248 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @pb3 

Hope this email finds you well,

Please note that the DDR Validation tool determine the results the ODT Validation.

The QCVS Tool is programmed to select a central value from among the passing cells.
This means that if all combinations pass validation,
QCVS will choose a value that lies at the center of the range of all passing cells.

Have a great day.

BR,

Hector V

0 Kudos
Reply