DDR4 clock (MCK) termination

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR4 clock (MCK) termination

2,220件の閲覧回数
trondwang
Contributor I

Hi NXP, in the reference design LS1043ARDB-PA/PB the termination resistor (R470 and R468) is 36 ohm for the differential clock.

The termination resistor for the single ended signals of the address bus/control  (R186+..) is 39 ohm.

Why do you use a lower resistance value for the differential signal.than for the adress bus/ control bus?

regards Trond Inge Wang

ラベル(1)
0 件の賞賛
返信
1 返信

2,072件の閲覧回数
ufedor
NXP Employee
NXP Employee

The termination circuit was simulated and optimized for the specific layout using HyperLynx.

Similar method is recommended for new designs.

0 件の賞賛
返信