DDR read/write issues custom board LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR read/write issues custom board LS1046A

32,223 Views
Rinke
Contributor II

Hi all,

 

I am in the process of trying to bring up a LS1046A board. Its a custom board based heavily off the Freeway design. The first step I am trying to do is get the connection diagnostics to pass with RCW override and DDR settings. D_INIT is cleared and its gets to the DDR memory access test. However when checking logs I can see that the DDR values do not match their expected values. See picture and logs(Read_Write_mem.txt). I see some resemblance of the expected values. D_Init_value is set to 0xDEADBEEF. 

 
 

Screenshot 2025-02-03 214119.png

Some things we tried and validated:

Hardware:

- Schematics reviewed and double checked

- Voltages are checked. GVDD, VREF, VTT and VPP

- Input and output DDR clocks

- DRAM reset signal is correct

- MEM enable signal is correct

Software:

- RCW correct and double checked. See below

- DQS skews are correct and double checked with schematics

- DQ mapping should be correct. Using the exact same layout as the Freeway board. See attached. 

 

Screenshot 2025-02-03 214611.png

 

I am unable to find a DDR config for the Freeway board. Is this something we can get to compare to our settings? Any pointers to what might be wrong? Im assuming its settings related since D_INIT is cleared and we are actually able to read/write to DDR. 

You can also find the logs below for the test for centering the clocks. Its ran with RCW override with the RCW mentioned below. CCS Output is also added. 

 

 

RCW:

RCWSR1:0x0810000d
RCWSR2:0x0a000000
RCWSR3:0x00000000
RCWSR4:0x00000000
RCWSR5:0x00000000
RCWSR6:0x40000002
RCWSR7:0x40000000
RCWSR8:0xc1000000
RCWSR9:0x00000000
RCWSR10:0x00000000
RCWSR11:0x00000000
RCWSR12:0x00000800
RCWSR13:0x00000000
RCWSR14:0x00000000
RCWSR15:0x00000096
RCWSR16:0x00000001

 

Any tips and/or pointers to potential fixes is appreciated. 

 

Rinke

0 Kudos
Reply
25 Replies

27,527 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following procedure to use QCVS DDRv tool to do DDR validation and optimization.

1. QCVS DDRv tool doesn't support RCW overriding function, you need to program RCW binary image to QSPI flash and configure the target board to boot from QSPI flash.

Please refer to section "8.6 Board Recovery" in C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf to program RCW to QSPI NOR flash.

In your description, your RCW configuration is incorrect. In your configuration, RCW[10-15] is 010000 (16:1), so DDR data rate is 1600MT/s, however you configure DDR data rate as 2100MT/s in QCVS DDRv project.

Please use the following method to build RCW binary image in your Linux host PC.

$ git clone https://github.com/nxp-qoriq/rcw.git

$ cd rcw

Then modify ls1046afrwy/NN_NNQNNPNP_3040_0506/rcw_1600_qspiboot.rcw according to your target board.

$ make

You will get ls1046afrwy/NN_NNQNNPNP_3040_0506/rcw_1600_qspiboot.bin, please program it to the beginning of your QSPI NOR flash.

 

2. Please refer to the attached DDR controller registers configuration file, which I read from LS1046AFRWY target board.

When creating a QCVS DDR project, in DDR configuration panel, please select configuration mode as "From memory file" and "Discrete DRAM" and specify the input file as the attached CodeWarrior Register Text file.

 

3. Please double click "DDR_mc1:DDR" to open Properties panel, please modify parameters in Properties panel according to your DDR datasheet and the schematics of your target board.

 

4. In the validation panel, please check all Validation stage and Operational DDR tests to connect to your target board to finish all the validations.

 

5. Please save the configuration and generate the latest code files from Project->Generate Processor Expert code. In "Generated_Code" folder, please use "ddr_init1.c" in ATF source code atf/plat/nxp/soc-ls1046a/ls1046afrwy, please use "ddrCtrl_1.py" in CodeWarrior initialization file.

0 Kudos
Reply

27,517 Views
Rinke
Contributor II

Thanks for the DDR config of the Freeway board!

 

1. If DDRv tool does not support RCW overriding. What it this setting for?

Screenshot 2025-02-06 102812.png

 

Thanks for the find in the RCW. Found it aswell and changed it to 2100. Does not make a difference. 

 

You point to ARMv8_Targeting_Manual.pdf section 8.6 for bringup of the board. This requires the flash manager to work. Flash manager requires the initialization file which requires DDR to function. So I first need to create a working DDR config before I can flash RCW right? 

 

0 Kudos
Reply

27,509 Views
yipingwang
NXP TechSupport
NXP TechSupport

The flash programmer is configured to use OCRAM(rather than DDR) in CodeWarrior, you could use CodeWarrior to program RCW to QSPI flash first.

Please refer to the following RCW configuration on LS1046AFRWY

Reset Configuration Word (RCW):
00000000: 0c150010 0e000000 00000000 00000000
00000010: 30400506 00800012 40025000 c1000000
00000020: 00000000 00000000 00000000 00038800
00000030: 20044100 24003101 00000096 00000001

0 Kudos
Reply

27,496 Views
Rinke
Contributor II

Thanks for the answer. Im trying to first flash the RCW into QSPI now. The flash manager indicates its able to correctly flash. Which is nice. 

The RCW im trying to write is attached. 

I am specifically not turning on any Serdes configurations to avoid issues with it. 

Now im trying to run the DDRv tool without RCW override. Then I get the following error:

#################### Result for: wrlvl_searcher ###### Run  1 ######################################

Test result: [
============================================================
Updated: WRLVL_CNTL = 0x86750605, WRLVL_CNTL_2 = 0x00000000, WRLVL_CNTL_3 = 0x00000000, SDRAM_CLK_CNTL = 0x02800000


Traceback (most recent call last):
  File "C:\Freescale\CW4NET_v2020.06\Common\QCVS\Optimization\resources\QorIQ\ARMv8/ddr/wrlvl_searcher.py", line 204, in write_leveling_start_searcher
    debug = ddr_init.read_debug_regs(ddr_ctrl, session)
  File "C:\Freescale\CW4NET_v2020.06\Common\QCVS\Optimization\resources\QorIQ\ARMv8\ddr\ddr_init.py", line 812, in read_debug_regs
    swap = (ddr_ctrl['endianness'][default_space] == 'little_endian')
KeyError: 'endianness'
]

Any pointers what to look for?

0 Kudos
Reply

27,479 Views
Rinke
Contributor II

Im also trying to run the initialization file without RCW override now. It was telling me to remove the RESET_REQ_B signal line from the reset cirquit to get a better error. After disconnecting I get this message. When I dump the contents of the QSPI memory I can see the contents of the RCW and preamble are all in the QSPI. Also when checking QSPI clock we can see a nice signal on boot being there. How do we solve this? 

 

Screenshot 2025-02-06 162954.png

 

0 Kudos
Reply

27,444 Views
yipingwang
NXP TechSupport
NXP TechSupport

For QSPI flash RCW, byte swap is required. However in the recent released SDK byte swap script is provide in ATF source code.  Please refer to the following procedure to generate ATF pbl image.

$ git clone https://github.com/nxp-qoriq/atf.git
$ cd atf
$ git checkout -b LSDK-21.08 LSDK-21.08

$ sudo apt-get install gcc-aarch64-linux-gnu

$ export CROSS_COMPILE=aarch64-linux-gnu-

$ make PLAT=ls1046afrwy bl2 BOOT_MODE=qspi pbl RCW=~/data/rcw/ls1046afrwy/NN_NNQNNPNP_3040_0506/test.bin

Note: please specify RCW binary path generated by you.

You will get build/ls1046afrwy/release/bl2_qspi.pbl, please program bl2_qspi.pbl at offset 0 of QSPI flash.

Please refer to the attached image generate with your RCW text file.

0 Kudos
Reply

27,357 Views
Rinke
Contributor II

Thanks for the help!

 

Is the ATF the only thing I need on the QSPI memory to be able to run the DDRv tool? Or would I also need BL2 and/or BL31/33? Is there a full instruction list to run the DDRv tool? 

0 Kudos
Reply

27,341 Views
yipingwang
NXP TechSupport
NXP TechSupport

After programing  bl2_qspi.pbl at offset 0 of QSPI flash, there is valid RCW on QSPI flash, then you could do DDRv validation. No need to deploy BL31/BL33 images.

0 Kudos
Reply

27,264 Views
Rinke
Contributor II

When flashing your exact file into QSPI nor flash and then running the ddrv tool I am still running into the endianness issue. Even when I build the pbl myself I have this issue. 

 

#################### Result for: wrlvl_searcher ###### Run  1 ######################################

Test result: [
============================================================
Updated: WRLVL_CNTL = 0x86750605, WRLVL_CNTL_2 = 0x00000000, WRLVL_CNTL_3 = 0x00000000, SDRAM_CLK_CNTL = 0x02800000


Traceback (most recent call last):
  File "C:\Freescale\CW4NET_v2020.06\Common\QCVS\Optimization\resources\QorIQ\ARMv8/ddr/wrlvl_searcher.py", line 204, in write_leveling_start_searcher
    debug = ddr_init.read_debug_regs(ddr_ctrl, session)
  File "C:\Freescale\CW4NET_v2020.06\Common\QCVS\Optimization\resources\QorIQ\ARMv8\ddr\ddr_init.py", line 812, in read_debug_regs
    swap = (ddr_ctrl['endianness'][default_space] == 'little_endian')
KeyError: 'endianness'
]

 

0 Kudos
Reply

27,252 Views
Rinke
Contributor II

Ive been trying some different RCW settings. I feel there were still some incorrect settings. This is my current RCW

RCWSR1:0x0c150010
RCWSR2:0x0e000000
RCWSR3:0x00000000
RCWSR4:0x00000000
RCWSR5:0x00000000
RCWSR6:0x00f00002
RCWSR7:0x40000000
RCWSR8:0xc1000000
RCWSR9:0x00000000
RCWSR10:0x00000000
RCWSR11:0x00000000
RCWSR12:0x00018800
RCWSR13:0x20024100
RCWSR14:0x00000000
RCWSR15:0x00000096
RCWSR16:0x00000001

When I put these settings into the RCW override function in the initialization file I can run the connection diagnostics tool and it will pas DDR initialization but then fail on read/write. Like i had before. I feel the issue is in getting this RCW on the board. 

I am converting above into the format below for building it in the ATF. 

/*
* LS1046AFRWY RCW for SerDes Protocol 0x3040_0x0506
*
* 4G configuration -- 4G QSGMII +  2 PCIe
*
* Frequencies:
*
* Sys Clock: 100 MHz
* DDR_Refclock: 100 MHz
*
* Core		-- 1600 MHz (Mul 16)
* Platform	-- 600 MHz (Mul 6)
* DDR		-- 2100 MT/s (Mul 21)
* FMan		-- 700 MHz (CGA2 /2)
* QSGMII	-- 100 MHz (5G)
* PCIE		-- 100 MHz (5G)
* eSDHC	-- 1400 MHz (CGA2 /1)
*
* Hardware Accelerator Block Cluster Group A Mux Clock:
*   FMan        - HWA_CGA_M1_CLK_SEL = 6 - Async mode, CGA PLL 2 /2 is clock
*   eSDHC, QSPI - HWA_CGA_M2_CLK_SEL = 1 - Async mode, CGA PLL 2 /1 is clock
*
* Serdes Lanes vs Slot information
*  Serdes1 Lane 0 (D) - Unused
*  Serdes1 Lane 1 (C) - Unused
*  Serdes1 Lane 2 (B) - QSGMII6,QSGMII5,QSGMII10,QSGMII1 port
*  Serdes1 Lane 3 (A) - Unused
*
*  Serdes2 Lane 0 (A) - Unused
*  Serdes2 Lane 1 (B) - PCIe2 Gen3 x1
*  Serdes2 Lane 2 (C) - Unused
*  Serdes2 Lane 3 (D) - PCIe3 Gen3 x1
*
* PLL mapping: 2222_2222
*
* Serdes 1:
*  PLL mapping: 2222
*
*  SRDS_PLL_REF_CLK_SEL_S1 : 0b'01
*    SerDes 1, PLL1[160] : 0 - 100MHz for QSGMII
*    SerDes 1, PLL2[161] : 1 - 100MHz for QSGMII
*  SRDS_PLL_PD_S1 : 0b'0
*    SerDes 1, PLL1 : 0 - not power down
*    SerDes 1, PLL2 : 0 - not poewr down
*  HWA_CGA_M1_CLK_SEL[224-226] : 6 - Cluster Group A PLL 2 /2 to FMan
*
* Serdes 2:
*  PLL mapping: 2222
*  SRDS_PLL_REF_CLK_SEL_S2 : 0b'00
*    SerDes 2, PLL1[162] : 0 - 100MHz for PCIe
*    SerDes 2, PLL2[163] : 0 - 100MHz for PCIe
*  SRDS_PLL_PD_S2 : 0b'00
*    SerDes 2, PLL1 : 0 - not power down
*    SerDes 2, PLL2 : 0 - not poewr down
*  SRDS_DIV_PEX_S2 : 0b'01
*    00 - train up to max rate of 8G
*    01 - train up to max rate of 5G
*    10 - train up to max rate of 2.5G
*
* DDR clock:
* DDR_REFCLK_SEL : 1 - DDRCLK pin provides the reference clock to the DDR PLL
*
*/
 
#include <../ls1046ardb/ls1046a.rcwi>
 
SYS_PLL_RAT=6
MEM_PLL_RAT=21
CGA_PLL1_RAT=16
CGA_PLL2_RAT=15
SRDS_PRTCL_S1=0
SRDS_PRTCL_S2=0
SRDS_PLL_PD_S1=3
SRDS_PLL_PD_S2=3
DDR_REFCLK_SEL=0
DDR_FDBK_MULT=2
PBI_src=4
IFC_MODE=37
HWA_CGA_M1_CLK_SEL=6
DRAM_LAT=1
UART_BASE=7
IRQ_OUT=1
IFC_GRP_A_EXT=1
IFC_GRP_E1_EXT=1
IFC_GRP_F_EXT=1
IFC_GRP_D_BASE=1
EC1=0
EC2=0
TVDD_VSEL=0
DVDD_VSEL=0
EVDD_VSEL=0
IIC2_EXT=0
SYSCLK_FREQ=600
HWA_CGA_M2_CLK_SEL=1
 
.pbi
// set CLK_SEL for QSPI CONFIG Register
write 0x57015c, 0x20100000
// set SCFG_SCRATCHRW1 ansd SCFG_SCRATCHRW2 for boot location ptr
write 0x570600, 0x00000000
write 0x570604, 0x40100000
.end
 
// Errta A-008850 for ddr controller for barrier transaction
#include <../ls1046ardb/cci_barrier_disable.rcw>
// Set USB PHY PLL for 100MHz
#include <../ls1046ardb/usb_phy_freq.rcw>
// Clear SerDes RxBoost on SD2 lane D
#include <../ls1046ardb/serdes_sata.rcw>
// Errata A-010477 and  A-008851 for PCI Express Gen3 link training
#include <../ls1046ardb/pex_gen3_link.rcw>
 
.pbi
// QSPI END_CFG 64 bit LE
write 0x550000, 0x000f400c
.end

 

This results in the attached bl2_qspi.zip. Which I load up into the board and run the connection diagnostics tool without overwriting RCW it results in this:

Rinke_0-1739486713040.png

Rinke_1-1739486737164.png



Any tips to what I am doing wrong? Could you have a look at the RCW and spot any mistakes? I am specifically settings SRDS_PLL_PD_S1 and S2 to turn off Serdes for now. 

 

Thanks!

0 Kudos
Reply

27,239 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please try the image bl2_qspi.pbl provided me again, I have verified it on LS1046AFRWY, I have passed all the diagnostics testing(including DDR read), then I sent it to you. I have attached it in this post again.

When you do flash programming, please remember to check erase action.

If you still have problem to use this image, please use flash programmer to dump the flash and save it to a file and send it to me.

0 Kudos
Reply

27,154 Views
Rinke
Contributor II

Thanks for testing. I flashed it using erase and verify. All good. 

Once i tried to run Centering the clock I get the same endianness error as before. 

 

 

#################### Result for: wrlvl_searcher ###### Run  1 ######################################

Test result: [
============================================================
Updated: WRLVL_CNTL = 0x86750605, WRLVL_CNTL_2 = 0x00000000, WRLVL_CNTL_3 = 0x00000000, SDRAM_CLK_CNTL = 0x02800000


Traceback (most recent call last):
  File "C:\Freescale\CW4NET_v2020.06\Common\QCVS\Optimization\resources\QorIQ\ARMv8/ddr/wrlvl_searcher.py", line 204, in write_leveling_start_searcher
    debug = ddr_init.read_debug_regs(ddr_ctrl, session)
  File "C:\Freescale\CW4NET_v2020.06\Common\QCVS\Optimization\resources\QorIQ\ARMv8\ddr\ddr_init.py", line 812, in read_debug_regs
    swap = (ddr_ctrl['endianness'][default_space] == 'little_endian')
KeyError: 'endianness'
]

 

 

I have attached the dump from my QSPI. 

 

fl_erase 0x0 0x9e00
Erased 39.50KB in 0.21s
fl_write 0x0 "C:\Users\Rinke\Downloads\bl2_qspi (1) (1)\bl2_qspi.pbl" --verify
Verify from 0x0 to 0x9dff succeeded
Wrote "C:/Users/Rinke/Downloads/bl2_qspi (1) (1)/bl2_qspi.pbl" in 0.77s
fl_dump 0x0 0x9dff -f "C:\Users\Rinke\Downloads\bl2_qspi (1) (1)\read_back_bl2.txt"
Dumped 39.50KB in 0.48s

 

 

 

0 Kudos
Reply

27,063 Views
yipingwang
NXP TechSupport
NXP TechSupport

No problem with your read back image.

After programming your read back image to my LS1046AFRWY demo board, I can perform the diagnose task and DDR Centering the clock validation successfully.

Please note you need to configure cfg_rcw_src[0:8] as 0_0100_010x to configure the target board boot from QSPI flash.

If your problem persists, please capture CCS console log to me to do more investigation.

After click "Start Validation" in QCVS DDR project, the CCS console will pop up in Windows task bar. Please open CCS and type "log v", then click "Start Validation" again, the low level CCS log will be printed out, please capture this log to me to do more investigation.

0 Kudos
Reply

27,032 Views
Rinke
Contributor II

Hi,

 

Yes the cfg_rcw_src[0:8] as 0_0100_010x is configured like this. Hereby attached the ccs log. 

 

0 Kudos
Reply

26,964 Views
yipingwang
NXP TechSupport
NXP TechSupport

There is problem with RCW loading. Please delete all PBI commands in your RCW configuration file to do verification.

The following RCW configurations are read from my target board, please try whether you could use these values to do RCW overriding with CodeWarrior.

RCWSR00: 0x0C150010

 

RCWSR01: 0x0E000000

 

RCWSR02: 0x00000000

 

RCWSR03: 0x00000000

 

RCWSR04: 0x00000000

 

RCWSR05: 0x00000002

 

RCWSR06: 0x40000000

 

RCWSR07: 0xC1000000

 

RCWSR08: 0x00000000

 

RCWSR09: 0x00000000

 

RCWSR10: 0x00000000

 

RCWSR11: 0x00000800

 

RCWSR12: 0x00000000

 

RCWSR13: 0x00000000

 

RCWSR14: 0x00000096

 

RCWSR15: 0x00000001

0 Kudos
Reply

26,954 Views
Rinke
Contributor II

When I use your exact RCW values I am getting this:

I emptied the QSPI memory before to make sure nothing is interfering. 

 

Screenshot 2025-02-19 131150.png

Your RCW itself does not work for me. Once I change RCW5 to 0x00f00002. So powering down the Serdes and uncommenting 6 (For selecting QSPI boot) it will work for me. 

 

        TA.rcw.set_data({1: 0x0C150010})
        TA.rcw.set_data({2: 0x0e000000})
        TA.rcw.set_data({3: 0x00000000})
        TA.rcw.set_data({4: 0x00000000})
        TA.rcw.set_data({5: 0x00000000})
        TA.rcw.set_data({6: 0x00f00002})
        #TA.rcw.set_data({7: 0x40000000}) 
        TA.rcw.set_data({8: 0xc1000000})
        TA.rcw.set_data({9: 0x00000000})
        TA.rcw.set_data({10: 0x00000000})
        TA.rcw.set_data({11: 0x00000000})
        # Configure UART
        TA.rcw.set_data({12: 0x00000800})
        # Configure QSPI
        TA.rcw.set_data({13: 0x00000000})
        TA.rcw.set_data({14: 0x00000000})
        TA.rcw.set_data({15: 0x00000096})
        TA.rcw.set_data({16: 0x00000001})

 

0 Kudos
Reply

26,843 Views
yipingwang
NXP TechSupport
NXP TechSupport

I generated file bl2_qspi.pbl with your RCW configuration, please extract the attached file and program it at offset 0 of your QSPI flash, and configure cfg_rcw_src[0:8] as 0_0100_0100, then do verification.

If your problem persists, please create a QCVS PBL project in CodeWarrior to check whether it is possible to read RCW from the target board.

 

0 Kudos
Reply

26,774 Views
Rinke
Contributor II

Hey 

 

So we got BL2 working. I needed to uncomment the first PBI instruction that was generic in the freeway config. We are using a different DRAM chip compared to the Freeway. Once we made some changes in BL2 we get the message below. Im assuming ddr controller initialized properly? I tried to run ddrv tool now but it doesnt do anything. 

Screenshot 2025-02-20 225652.png

 

Err. capture registers:
0xE20, 0x00000000     0xE24, 0x00000000     0xE28, 0x00000000     0xE40, 0x00000080     
0xE44, 0x00000000     0xE48, 0x00000000     0xE4C, 0x00000000     0xE50, 0x00000000     
0xE54, 0x00000000     0xE58, 0x00010000     


Dump:
0xF00, 0x00000000     0xF04, 0x00003002     0xF08, 0x00000010     0xF0C, 0x14000C20     
0xF10, 0x00000000     0xF14, 0x00000000     0xF18, 0x00000000     0xF1C, 0x00000000     
0xF20, 0x00000000     0xF24, 0x10101010     0xF28, 0x10101010     0xF2C, 0x10101010     
0xF30, 0x10101010     0xF34, 0x10103000     0xF38, 0x00000000     0xF3C, 0x00000000     
0xF40, 0x00000000     0xF44, 0x00000000     0xF48, 0x00000001     0xF4C, 0x94000000     
0xF50, 0x3C003B00     0xF54, 0x3D003D00     0xF58, 0x30003000     0xF5C, 0x31003200     
0xF60, 0x2F000000     0xF64, 0x00009000     0xF68, 0x00000021     0xF6C, 0x00000000     
0xF70, 0x0080006A     0xF74, 0x00000000     0xF78, 0x00000000     0xF7C, 0x00000000     
0xF80, 0x00000000     0xF84, 0x00000000     0xF88, 0x00000000     0xF8C, 0x00000000     
0xF90, 0x00000000     0xF94, 0x80000000     0xF98, 0x00000000     0xF9C, 0x02020202     
0xFA0, 0x02020202     0xFA4, 0x02020202     0xFA8, 0x02020202     0xFAC, 0x02020000     
0xFB0, 0x00000003     0xFB4, 0x1F1F1F1F     0xFB8, 0x1F1F1F1F     0xFBC, 0x1F1F1F1F     
0xFC0, 0x1F1F1F1F     0xFC4, 0x1F1F1F1F     0xFC8, 0x1F1F1F1F     0xFCC, 0x1F1F1F1F     
0xFD0, 0x1F1F1F1F     0xFD4, 0x1F1F1F1F     0xFD8, 0x1F1F1F1F     0xFDC, 0x1F1F1F1F     
0xFE0, 0x1F1F1F1F     0xFE4, 0x1F1F1F1F     0xFE8, 0x1F1F1F1F     0xFEC, 0x1F1F1F1F     
0xFF0, 0x1F1F1F1F     0xFF4, 0x1F1F1F1F     0xFF8, 0x1F1F1F1F     0xFFC, 0x1F004740     



Data: 
0x00000005 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 

]

 When I check ccs logv it just gets stuck on the next line. See CCS log for full log

read_memory(coreh.{serverh=0,cc_index=0,chain_pos=17},
  addr.{addr_hi=0x00000000,addr_lo=0x01080114,size=4,space=4607},count=4,*data)
  data: 00401052

 

0 Kudos
Reply

26,501 Views
yipingwang
NXP TechSupport
NXP TechSupport
  1. When creating a QCVS DDR project, in DDR configuration panel, please select configuration mode as "From memory file" and "Discrete DRAM" and specify the input file as the attached CodeWarrior Register Text file.

 

  1. Please double click "DDR_mc1:DDR" to open Properties panel, please modify parameters in Properties panel according to your DDR datasheet and the schematics of your target board.

      Then save the configurations to do DDR validation.

0 Kudos
Reply

26,184 Views
Rinke
Contributor II

Does not make a difference. Can you tell me exactly in what state the board should be in to run the DDRv tool? When running just BL2 the cpu gets stuck trying to load BL3. Logically. But is that oke for the DDRv tool? D_Init is cleared by our BL2 so the ddr controller should be initialized for the ddrv tool to take over? When running BIST in BL2 it fails on training. Any tips?

ERROR:   Found training error(s): 0x3002
ERROR:   Writing DDR register(s) failed 0
ERROR:   Programing DDRC error
INFO:    DRAM size 0xfffffffffffffffb
ERROR:   DDR init failed.

 

0 Kudos
Reply