DDR: ISSI vs Micron

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,931件の閲覧回数
andychernock
Contributor III

Micron MT40A512M16JY-083E-AAT-B vs  ISSI  IS46QR16512A-083TBLA2

If we calibrate/test/pass our design using the Micron DDR4...

...would you know if this ISSI DDR4 will work without any driver changes to our LS1046A?

 

Checking if others may have done this already when replacing the EOL Micron -083 DDR4.

I hope it will drop in and work using the calibration settings for the Micron DDR4 -083 speed grade.

Note that the operating speed is 1600Mt/s in our LS1046A design.

 

 

0 件の賞賛
返信
1 解決策
2,926件の閲覧回数
Bulat
NXP Employee
NXP Employee

We do not have such reports from customers. Basically timing parameters of different SDRAM manufacturers are very close to each other, most probably setup changing will not be needed. Anyway, it would be advisable to run DDR validation tool with new memory devices to confirm/validate memory settings.

Regards,

Bulat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,927件の閲覧回数
Bulat
NXP Employee
NXP Employee

We do not have such reports from customers. Basically timing parameters of different SDRAM manufacturers are very close to each other, most probably setup changing will not be needed. Anyway, it would be advisable to run DDR validation tool with new memory devices to confirm/validate memory settings.

Regards,

Bulat

0 件の賞賛
返信