Curious about PCIE legacy interrupt...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Curious about PCIE legacy interrupt...

1,789 Views
gyosunshim
Contributor III

Hello,

I am using LS104x custom CPU.

PCIe legacy interrupt supports a total of 4 INTA-INTDs.

Question.

1. Do you know the history of why only 4 applications were applied?

2. Is there any problem even if the 3 PCIE ports of the LS1046 are set to the same interrupt INTA?

Thank you.

Best Regards,

Gyosun.

0 Kudos
Reply
2 Replies

1,786 Views
ufedor
NXP Employee
NXP Employee

1) What does it mean: "4 applications were applied"?


2) There is no problem - refer to the QorIQ LS1046A Reference Manual, Table 5-1. Interrupt Assignments.

0 Kudos
Reply

1,782 Views
gyosunshim
Contributor III

Hi Ufedor,

 

Legacy Interrupt consists of only 4 INTA-INTDs.

I would like to know why I configured only 4 interrupts when designing the specification at first.

No matter how much I googled, I was curious because there was no data explaining the history.

 

Thank you,

Best Regards,

Gyosun.

0 Kudos
Reply