'libtsn.so' issue on board LS1028A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

'libtsn.so' issue on board LS1028A

614 Views
Mereye
Contributor I

Hello,

I have built a linux version with tsntool enabled, I called this file "ub2.itb" and save it to an USB to use it I did the following: Powerup the board and stop it at u-boot.

>usb start

>load usb 0:1 0xa0000000 ub2.itb

>bootm 0xa0000000#ls1028ardb

ran the tsntool program but when I try to perform some test as said the user guide LSDKUG_Rev19.09_311219 on section 8.7.1.3.2.1 Basic gates closing, line "cp libtsn.so /lib" I receive the issue "cp: cannot stat 'libtsn.so' No such file or directory. Why I'm receiving this error?

thank you in advance

 

 

0 Kudos
Reply
1 Reply

601 Views
yipingwang
NXP TechSupport
NXP TechSupport

Which version LSDK do you use now?

Did you build ub2.itb with flex-builer?

How did you enable tsntool and build ub2.itb?

 

0 Kudos
Reply