Cross compile with gdb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Cross compile with gdb

跳至解决方案
3,301 次查看
bladerunner1010
Contributor III

which toolchain should I use?

0 项奖励
回复
1 解答
3,276 次查看
Pavel
NXP Employee
NXP Employee

LSDK recommends the following toolchain:

gcc-linaro-4.9-2016.02-x86_64_aarch64-linux-gnu–

 

See LSDK User Guide.

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,288 次查看
Pavel
NXP Employee
NXP Employee

1. NXP offers LSDK 2108 for the LS1043ARDB board:https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/layerscap... See the Chapter 4.1.9 in LSDK 2108 User Guides:https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev21.08.pdf This Chapter contains documentation for building and deploying LSDK on the LS1043a board. LSDK 2108 recommends using the following toolchain:

gcc-linaro-4.9-2016.02-x86_64_aarch64-linux-gnu– Used to compile UEFI firmware (can be downloaded from: https://releases.linaro.org/components/toolchain/binaries/4.9-2016.02/aarch64-linuxgnu/gcclinaro-4.9...)

0 项奖励
回复
3,294 次查看
bladerunner1010
Contributor III

which toolchain?

 

0 项奖励
回复
3,277 次查看
Pavel
NXP Employee
NXP Employee

LSDK recommends the following toolchain:

gcc-linaro-4.9-2016.02-x86_64_aarch64-linux-gnu–

 

See LSDK User Guide.

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf

0 项奖励
回复