Cortex-A7: Core not responding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cortex-A7: Core not responding

2,324 Views
jaroslavdytrych
Contributor I

Hello All.

We have own board with a LS1020A and there are problems with a linux stability. So we want to run a DDR validation but we have a problem with connecting to the processor using CW QCVS and CodeWarrior TAP.

CCS command output

(bin) 44 % dele a
(bin) 45 % config cc cwtap
(bin) 46 % ccs::config_chain {ls1020a dap sap2}
(bin) 47 % display ccs::get_config_chain
Chain Position 0: LS1020A
Chain Position 1: CoreSight ATB Funnel
Chain Position 2: CoreSight TMC
Chain Position 3: CoreSight TMC
Chain Position 4: CoreSight TMC
Chain Position 5: CoreSight CTI
Chain Position 6: CoreSight CTI
Chain Position 7: CoreSight CTI
Chain Position 8: CoreSight ATB Funnel
Chain Position 9: Cortex-A7
Chain Position 10: Cortex-A7 PMU
Chain Position 11: Cortex-A7
Chain Position 12: Cortex-A7 PMU
Chain Position 13: CoreSight CTI
Chain Position 14: CoreSight CTI
Chain Position 15: Cortex-A7 ETM
Chain Position 16: Cortex-A7 ETM
Chain Position 17: DAP
Chain Position 18: SAP2
(bin) 48 % ccs::reset_to_debug
Cortex-A7: Core not responding

CCS Scan TAP output
(bin) 25 % source IDcode.tcl

TDO -----
        |
        * Device 0  IDCODE: 5BA00477  Device: Unknown Device
        * Device 1  IDCODE: 16B0001D  Device: FSL LS1 Device rev 2.x
        |
TDI -----

CW Target Connection output
check_min_version(serverh=0,*version)
  api version: 00000004 00000006
available_connections(serverh=0,*count,*cc)
  connections: {0,73,0xc0a801db}
cc_version(serverh=0,cc_index=0,index=0,*version)
config_server(config_reg=0,config_data=0x000027F6)
config_chain(serverh=0,cc=0,count=3,*devlist,*generic)
  devlist: ls1020a,dap,sap2
reset_to_debug(serverh=0,cc=0)
  ERROR(39): Subcore error encountered during multicore operation
parse_error_ext(coreh.{serverh=0,cc_index=0,chain_pos=0}, 39)
  error: Cortex-A7: Core not responding

Any idea what's wrong?

Maybe incorrect JTAG wiring?

Thanks for any help.

Labels (1)
0 Kudos
Reply
2 Replies

2,093 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Jaroslav Dytrych,

CCS failed at ccs::reset_to_debug, probably there is problem with RCW or JTAG interface hardware design on your target board.

1. Please refer to the section "4.4.6.2 Hard-coded RCW options" in LS1021A Reference Manual to configure your target board to use one hard-coded RCW, then verify your above CCS commands.

2. Please check the hardware design, please download "AN4878, QorIQ LS1021A Design Checklist - Application Note" from QorIQ LS1021A Dual-Core Communications Processor wi|NXP , and refer to "Figure 31. JTAG interface connection" to check your JTAG interface design, especially nRESET pin.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,093 Views
jaroslavdytrych
Contributor I

Hello Yiping Wang,

you are right. The problem was incorrect wiring JTAG (nRESET pin) on our target board. Now the problem was solved and the DDR validation tool works.

Thanks for your help.

Regards

Jarda.

0 Kudos
Reply