Console port accessing issue with LS1021ATSN-PA from Windows 10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Console port accessing issue with LS1021ATSN-PA from Windows 10

3,234 次查看
Abhilash_PV
Contributor I

Hi,

I'm working on a LS1021ATSN-PA development board. I'm facing an issue with its console port access from my Windows 10 PC. As mentioned in the quick start guide, I've connected the board's Micro USB console port to my PC using the Micro-B USB cable. The cable connection detected at the PC and appeared as a USB Mass Storage Device under the USB controllers of the Device Manager. But it does not appear as a COM port. I found a note from the MBED saying that Windows 10 does not require a specific serial driver to enable the COM port, however an older version of Windows 8 or lesser requires it. In my Windows 10 PC I cannot find the virtual COM port corresponding to this USB connection.

How do I resolve the issue? Kindly help me to proceed on it. 

Thank You.

标签 (1)
0 项奖励
回复
8 回复数

2,255 次查看
Youngsoo_do
Contributor III

Any solution to this problem?

0 项奖励
回复

3,218 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached document to write CMSIS-DAP firmware image k22fx512_if_mbed.bin on  your target board.

0 项奖励
回复

3,208 次查看
Abhilash_PV
Contributor I

Thank you for the response.

I have followed the steps mentioned in the document to update CMSIS-DAP firmware on the board and it updated successfully. However I could not get the console port appeared as virtual COM port on my Windows10 PC. I have also tried the workaround suggested in one of the community question links (https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798002?commentID=10...) but it didn't help me either. On my PC I'm still getting it as USB Mass Storage Device only, and in the Teraterm application I cannot select the virtual COM port to connect with the board's console port. 

0 项奖励
回复

3,190 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please make sure that you used CMSIS-DAP firmware image k22fx512_if_mbed.bin.

Please refer to the section "5. Windows mbed USB driver" in the document to install mbed USB driver.

There is a known issue with MBED operation under Windows 10:

        https://os.mbed.com/blog/entry/DAPLink-bootloader-update/

        This is the workaround we have confirmed to fix the mbed issue on Windows 10 PC's:

        - Go to the "Start" option on the PC and type the command  " services.msc"

        - Than you should see the following "Services" window open

        - Select the "Storage Services" and on the left-hand side of the window click the "Stop the service"

0 项奖励
回复

3,153 次查看
Abhilash_PV
Contributor I

I've followed the same steps mentioned along with the Windows 10 workaround procedure. But it did not solve my issue. 

After copying CMSIS-DAP firmware image "k22fx512_if_mbed.bin" into the "BOOTLOADER" named drive, the 'K22' marked status LED on the board blinks very fast. Then on unplugging and re-plugging of USB cable caused a drive named "MBED" appears on my PC. No virtual COM port is being created corresponding to the console port. I have re-enabled "Storage Services" in my PC and checked again. No difference observed (Only "MBED" drive appeared and no virtual COM port). 

MBED DriveMBED Drive

I have noticed a file named "fail.txt" in the "MBED" drive path as shown above. Content inside the text file is "SWD ERROR".

Am I right in the procedure that I followed? Is there any other image I've to use further to the above procedure?

0 项奖励
回复

3,145 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please try the attached firmware image.

After plug in USB cable, please wait for while until the system is stable.

0 项奖励
回复

3,141 次查看
Abhilash_PV
Contributor I

I have tried this one but no difference in behavior observed. 

0 项奖励
回复

2,894 次查看
reginaldstjohn
Contributor III

We are seeing the same issue. Installed the k22fx512_if_mbed.bin, turned off the service "Storage Service" (There is no Storage Services),

Still no com port showing up in Windows 10 as of Oct-2021

0 项奖励
回复