Compatible SODIMM for LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compatible SODIMM for LS1046A

1,762 Views
carljones
Contributor III

Hello @ufedor ,

I would like to confirm if this SODIMM is compatible with LS1046A 

- CT8G4SFRA266.C8FP

I have read from LS1046APB.pdf that speed supported by LS1046A is up to 2100 MT/s but I see that some 2400 MT/s SODIMMs work. That's why I wanted to confirm if the above SODIMM (2666 MT/s) will work as well.

Kind regards,

Carlos

0 Kudos
Reply
2 Replies

1,700 Views
yipingwang
NXP TechSupport
NXP TechSupport

the maximum data rate that LS1046A supports is 2100 MT/s.
the SoDIMM also has speed bin rating that can be 2666 MT/s or 3200 MT/s, or ...

Any SoDIMMs that claim to be JEDEC compliant with speed bin rating of higher than 2100 MT/s would work with LS1046A.

0 Kudos
Reply

1,678 Views
carljones
Contributor III

Thank you for the confirmation @yipingwang 

Kind regards

0 Kudos
Reply