Codewarrior development environment issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior development environment issues

1,621 Views
13540372905
Contributor I

We used FRWY-LS1012 for the project, and use the CodeWarrior Development Suites for Networked Applications v11.4.0 environment ,when connected to the  CodeWarrior TAP a Error occurred that : 'ASCII' codec can't encode characters in position 21-26: ordinal not in range(128) '  , could you please help provide a codewarrior development environment  and corresponding instructions supporting FRWY-LS1012 board,thank you 

0 Kudos
Reply
2 Replies

1,550 Views
Pavel
NXP Employee
NXP Employee

Test your connection to your board using the following commands in CCS:

config cc cwtap

show cc

 

and

 

log v

source IDcode.tcl

 

See the following page:

https://community.nxp.com/docs/DOC-94804


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,550 Views
13540372905
Contributor I

Please help us analyze it as soon as possible, thank you

0 Kudos
Reply