Codewarrior TAP does not connect to target hardware under Ubuntu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior TAP does not connect to target hardware under Ubuntu

3,094 Views
DaT63
Contributor II

My configuration:

Target: NXP LS1046ARDB

JTAG Probe: CodeWarrior TAP (USB)

Host PC: Ubuntu 22.04 with CodeWarrior Development Studio 11.5.12

I am not able to perform a target connection under Ubuntu. I attach one screenshot of the Connection Server and one of the Diagnostic Output. Both Ubuntu and CodeWarrior have been updated.

I made a test with the Windows version of the CodeWarrior Development Studio and  the connection establishes without problems, so the hardware is working. Needless to say that I need to use Ubuntu so I need to find a solution

0 Kudos
Reply
1 Reply

3,066 Views
Oswalag
NXP TechSupport
NXP TechSupport

There are some issues regarding CWTAP under Ubuntu, Please refer to the attached workaround and let me know if it works on your side.

0 Kudos
Reply