Codewarrior/LS1043A memory access error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior/LS1043A memory access error

7,319 次查看
yoshida08
Contributor I

I am debugging a our designed board on which LS1043A is mounted.
I'm using code warrior to debug, but I get an error like the attachment.
What is the cause? 

0 项奖励
回复
7 回复数

7,080 次查看
yoshida08
Contributor I

Thank you for your reply.

I'm sorry, I reply late.

0 项奖励
回复

7,240 次查看
yoshida08
Contributor I

We solved problem of the JTAG hardware interface design.

We send new log.

This problem remain yet. 

0 项奖励
回复

7,219 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please configure the switch setting on your custom board to configure it as hard-coded RCW, then try whether CCS still failed at reset_to_debug.

If the problem remain, further investigating about JTAG interface hardware design is needed.

0 项奖励
回复

7,255 次查看
yoshida08
Contributor I

Thank you for your reply.

This problem remain yet. We checked our JTAG hardware interface design.

"nRESET" signal is connected to TRST direct. 

Is this connection a problem?

0 项奖励
回复

7,284 次查看
yipingwang
NXP TechSupport
NXP TechSupport

When you execute the Connection Diagnostics action, then CodeWarrior Connection Server(CCS) will be popped up automatically on the right bottom of the Windows task bar.

Please open CCS console, type "log v", then execute Connection Diagnostics again, the low level CCS log will be printed out, please capture the log to me to do more investigation.

0 项奖励
回复

7,277 次查看
yoshida08
Contributor I

Thank you for your reply.

we got the log.

Please check the attached file.

0 项奖励
回复

7,267 次查看
yipingwang
NXP TechSupport
NXP TechSupport

In your CCS log, it failed at "reset_to_debug".

Please make sure SERDES REF CLK is set to 100 MHz, set rcw_src to the hard-coded RCW option matching the board's DIP SW regarding SYSCLK and differential/single-ended clock source

If this problem remains, please check your JTAG hardware interface design.

Please refer to "Figure 18. JTAG interface connection" in the attached application note.

Please refer to "5.28 JTAG pin termination recommendations" in the attached app note.

0 项奖励
回复