Codewarrior Connection Diagnostics Runs Infinitely

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior Connection Diagnostics Runs Infinitely

1,608件の閲覧回数
Hasan0
Contributor I

Hello,

 

I am using LS1043ARDB development board with CodeWarrior TAP. I can debug and step through default bare-board Hello World project, which means the hardware works fine. However, when I click on "Diagnose Connection" button from Target Connections view, no output is displayed and the progress bar runs infinitely. 

 

I have tried different configuration settings including the default ones but the result didn't change. 

 

Here are some version information if that helps:

Codewarrior IDE version:
Version: 11.5.0 Build Id: 200629GA

Codewarrior Tap version:
900-76173 Rev H

Codewarrior TAP Firmware boot loader version:
Boot Loader Version: 1.0.1
OS Version: 1.0.5


By the way, a very similar question was asked before but was left unresolved. I didn't know whether to reply the existing thread or create a new one.: https://community.nxp.com/t5/Layerscape/LS1028ARDB-CodeWarrior-TAP-connects-but-will-not-return/td-p...

 

Looking for advice.

Thanks.

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,480件の閲覧回数
Hasan0
Contributor I

Hello,

Thank you for your answer June. However, before trying the solution you suggested, simply reinstalling the current version of IDE have worked. Probably, there was some problem with the installation. 

0 件の賞賛
返信

1,471件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

That's great, thanks for sharing.

0 件の賞賛
返信

1,520件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

Please kindly update your CodeWarrior IDE from 11.5.10 to 11.5.12.

 

My NXP Account->Software->Software Licensing and Support->View accounts->Product List->CodeWarrior for QorIQ LS Series ARMv8 ISA->

Please download update package

com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip

Please open CodeWarrior from C:\Freescale\CW4NET_v2020.06\CW_ARMv8\fsl_eclipse.bat, and install the update package from Help->Install New Software->Add->Archive.

 

And try to connect the CWTAP with ethernet:

Is the CCS, please kindly run the command below:

(bin) 7 % delete all

(bin) 8 % config cc cwtap:10.193.21.52 //(it's your CWTAP ethernet IP)

(bin) 9 % show cc

(bin) 10 % ccs::config_chain {ls1043a dap sap2}

(bin) 11 % display ::ccs::get_config_chain

 

If it could not solve your issue, please let me know your logs.

Thanks