CodeWarrior development studio target initialization file user guide

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior development studio target initialization file user guide

1,565件の閲覧回数
scottwelsh
Contributor II

I need to understand what parameter values to send to the fl.add_device() routine within the Target Initialization File. Please send me a link to a CodeWarrior Development Studio Target Initialization File User Guide or the like.

Thank you,

Scott

0 件の賞賛
返信
2 返答(返信)

1,532件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

I hope this post finds you well,

As you can see in the following example of fl.add_device

        fl.add_device({"alias": "qspi", "name": "MT25QU128ABA", "address": 0x40000000, "ws_address": 0x10000000, "ws_size": 0x1FFFF, "geometry": "8x1", "controller": "QSPI"})

        #set QSPI as current device

        fl.set_current_device("qspi")

The fl.add_device() is formed by the following characteristics

  • Alias: This setting specified the type of memory that is being used or you want to add.
    1. qspi
    2. sd
    3. mmc
    4. nor
    5. nand
  • Name: This setting specified the model or the number part of the memory or flash memory that you used or added
  • Address: This setting specified the base address in SoC for flash device.
  • Ws_address: This setting is for the workspace address; Address where the flash algorithm is downloaded.
  • Ws_size: This setting is for the size of the workspace.
  • Geometry: This setting specified the flash organization
  • Controller: This part specified the controller of the memory
    1. If you use qspi the controller would be QSPI
    2. If you use sd or mmc the controller is eSDHC
    3. If you use nor or nand the controller is IFC

Best regards,

Sebastian

0 件の賞賛
返信

1,547件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hello @scottwelsh,

I would like to inform you that I'm working on your question, I will let you know as soon as I have an update.

Thank you so much for your patience

Regards,

Sebastian

0 件の賞賛
返信