CodeWarrior / TAP / LS1046ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior / TAP / LS1046ARDB

ソリューションへジャンプ
3,140件の閲覧回数
Daves_Garage
Contributor IV

I cannot connect to my TAP module from CodeWarrior.  I am receive a "Problem Occurred" pop-up window that states 'Launching LS1046A_RDB(1)_Connect' has encountered a problem.  Program file not specified.  This occurs when I use the flash icon in the Target Connection Configuration window.

Any pointers would be very appreciated.

0 件の賞賛
返信
1 解決策
3,117件の閲覧回数
Daves_Garage
Contributor IV
0 件の賞賛
返信
2 返答(返信)
3,118件の閲覧回数
Daves_Garage
Contributor IV
0 件の賞賛
返信
3,129件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "3.2 Working with bareboard application" in C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf to create a bareboard project in CodeWarrior IDE to connect to the target board.

0 件の賞賛
返信