CodeWarrior / TAP / LS1046ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior / TAP / LS1046ARDB

Jump to solution
3,164 Views
Daves_Garage
Contributor IV

I cannot connect to my TAP module from CodeWarrior.  I am receive a "Problem Occurred" pop-up window that states 'Launching LS1046A_RDB(1)_Connect' has encountered a problem.  Program file not specified.  This occurs when I use the flash icon in the Target Connection Configuration window.

Any pointers would be very appreciated.

0 Kudos
Reply
1 Solution
3,141 Views
Daves_Garage
Contributor IV
0 Kudos
Reply
2 Replies
3,142 Views
Daves_Garage
Contributor IV
0 Kudos
Reply
3,153 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "3.2 Working with bareboard application" in C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf to create a bareboard project in CodeWarrior IDE to connect to the target board.

0 Kudos
Reply