Code Signing Tool with a Hardware Security Module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Signing Tool with a Hardware Security Module

Jump to solution
977 Views
endrunner_smw
Contributor III

I am aware that there are multiple versions of the code signing tool from different locations.

I currently am using the CST located at github.com/nxp-qoriq/cst. This appears to be version 2.0 and matches what documentation I seem to come across. I have also seen versions in the 3.* range as well as a 4.* version. From postings on the forums it seems these version 3 and 4 versions of CST can support a HSM through some configuration changes.

However, I can't seem to find an equivalent for CST 2.0? Can CST 2.0 utilize a HSM? If yes what steps would be required, if no, then can other versions of CST be used as drop in replacements?

I also noticed that the latest CST 4 doesn't appear to have actual source code available, or am I just looking in the wrong place? The precompiled binaries are only available for x86_64, but I'm developing natively on the LS1043A aarch64, so the precompiled binaries are obviously not an option. I don't mind building a different version, I just need to know where the source is and if there are any compatibility issues to be aware of?

Thank you for your time.

Tags (3)
0 Kudos
Reply
1 Solution
904 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

CST 2.0 does not have documented native HSM/PKCSsupport; for Layerscape the supported path is detached external signing with --img_hash plus sign_embedding , while i.MX CST 3.x/newer adds HSM features but is not verified as a drop-in replacement for QorIQ CST 2.0.

 

Regards

View solution in original post

0 Kudos
Reply
1 Reply
905 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

CST 2.0 does not have documented native HSM/PKCSsupport; for Layerscape the supported path is detached external signing with --img_hash plus sign_embedding , while i.MX CST 3.x/newer adds HSM features but is not verified as a drop-in replacement for QorIQ CST 2.0.

 

Regards

0 Kudos
Reply