Cannot clone the LSDK 1906 U-Boot source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot clone the LSDK 1906 U-Boot source

1,256 Views
yeah
Contributor II

The LSDKUG_Rev19.06.pdf says:

5.2.4.2 How to compile U-Boot binary
You need to compile the u-boot.bin binary to build the fip.bin binary.
Clone the u-boot repository and compile the U-Boot binary for TF-A.
1. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git
2. $ cd u-boot
3. $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-19.06
LSDK-19.06

But it failed at the clone stage:

git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git
Cloning into 'u-boot'...
remote: Counting objects: 638687, done.
remote: Compressing objects: 100% (102295/102295), done.
remote: Total 638687 (delta 528448), reused 637805 (delta 527779)
Receiving objects: 100% (638687/638687), 106.01 MiB | 4.96 MiB/s, done.
Resolving deltas: 100% (528448/528448), done.
warning: remote HEAD refers to nonexistent ref, unable to checkout.

Could you help on this?

0 Kudos
Reply
1 Reply

1,156 Views
Pavel
NXP Employee
NXP Employee

It looks like that LSDK 1906 is not completely installed on your Ubuntu 18.

Use the following command sequence for LSDK 19.06 installing:

sudo apt-get install git

 

tar xvzf flexbuild_lsdk1906.tgz

 

source setup.env

Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply