Cannot clone repos from source.codeaurora.org

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot clone repos from source.codeaurora.org

8,885件の閲覧回数
jopado
Contributor I

I am trying to get kernel and uboot source for Layerscape 18.03. Instructions from LSDK-KC-REV18.03.pdf chapter 7. Anyone else having issues?

user@ls1046:~$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux
Cloning into 'linux'...
remote: Counting objects: 6194997, done.
remote: Compressing objects: 100% (18195/18195), done.
remote: Total 6194997 (delta 51131), reused 60145 (delta 49138)
Receiving objects: 100% (6194997/6194997), 1.06 GiB | 844.00 KiB/s, done.
Resolving deltas: 100% (5201161/5201161), done.
Checking connectivity... done.
warning: remote HEAD refers to nonexistent ref, unable to checkout.

user@ls1046:~$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot
Cloning into 'u-boot'...
remote: Counting objects: 563314, done.
remote: Compressing objects: 100% (1422/1422), done.
remote: Total 563314 (delta 1829), reused 2091 (delta 1492)
Receiving objects: 100% (563314/563314), 94.86 MiB | 1.01 MiB/s, done.
Resolving deltas: 100% (465361/465361), done.
Checking connectivity... done.
warning: remote HEAD refers to nonexistent ref, unable to checkout.

0 件の賞賛
返信
5 返答(返信)

6,729件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use the following command sequence for flex-builder of the LSDK 18.03:

1.

source setup.env

2.

flex-builder -c firmware -a arm64


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,727件の閲覧回数
jopado
Contributor I

Lets try this again. Please see section 7 of the LSDK 18.03 Documenation,

specifically the following. The git clone does not work. Is this the

correct repo? Is the documentation wrong? What is the URL to the coreect

repo please.

0 件の賞賛
返信

6,727件の閲覧回数
stuartrubin
Contributor III

@Joe Dougherty, I'm having the same issue. Was this even resolved? Thanks 

0 件の賞賛
返信

6,727件の閲覧回数
jopado
Contributor I

I was able to use this to get the source:

   git clone https://github.com/qoriq-open-source/linux.git

   cd linux
   git checkout tags/LSDK-18.03-V4.14

Hope this helps.

0 件の賞賛
返信

6,727件の閲覧回数
stuartrubin
Contributor III

Thanks, Joe, I'll try it now.

0 件の賞賛
返信