Can we create a x86 VM using QEMU on LS2088ARDB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we create a x86 VM using QEMU on LS2088ARDB?

1,706件の閲覧回数
jaytirthkhairat
Contributor I

I have a software which requires CentOS 6.5 (x86). I want to run this software on NXP LS2088ARDB reference board. Porting is becoming increasingly difficult and time consuming. I am thinking of running CentOS 6.5 (x86) as a virtual machine on NXP LS2088ARDB reference board.  The 'QorIQ LS2088A BSP v0.2' manual mentions only of creating a ARM based virtual machine using QEMU. How do I create a x86 VM using QEMU on LS2088ARDB?

ラベル(1)
0 件の賞賛
返信
1 返信

1,137件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Theoretically, QEMU is emulator and it can emulate one architecture on another.

However, looking our SDK documentation I see we have only qemu-system-arm and qemusystem-aarch64, so this means in our SDK we support only ARM


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信