Can LS1046 update the program without uboot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can LS1046 update the program without uboot?

1,223 次查看
Hmc510
Contributor II

I noticed that LS1046 supports two startup modes:TF CARD/ QSPI FLASH.

Can LS1046 update the program without uboot? 

For example, The QSPI Flash is erased. Is there any other way to program firmware image without using the TF card boot mode.

 

Thanks

0 项奖励
回复
2 回复数

1,190 次查看
stadium_aquino
Contributor IV
0 项奖励
回复

1,206 次查看
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

With the CodeWarrior TAP, you have to boot the board from RAM and then you can use the flash programmer tool in CodeWarrior.

Search | NXP Semiconductors

0 项奖励
回复