Cache Locking on LS2080A/LS2085A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cache Locking on LS2080A/LS2085A

3,017件の閲覧回数
renatomancuso
Contributor I

Hello,

I was wondering if cache locking is available on any of the cache levels (L1, L2 or CPC) of the LS2080A or LS2085A platforms.

Also does this SoC include any performance monitoring unit similar to the EPU in QorIQ Pxxx platforms?

Thanks in advance for your answer.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,756件の閲覧回数
renatomancuso
Contributor I

Great. Can the L3 also be configured as SRAM like in the P4080?

Thanks!

0 件の賞賛
返信

2,756件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at ARM community:

https://community.arm.com/thread/5122

The ARM Cortex-A57 does not support locking of the L1 or L2 cache, see these pages of the Technical Reference Manual:

ARM Cortex-A57 MPCore Processor Technical Reference Manual: 6.1. About the L1 memory system

ARM Cortex-A57 MPCore Processor Technical Reference Manual: 7.1. About the L2 memory system


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,756件の閲覧回数
renatomancuso
Contributor I

Yes, I am aware of that. However, the LS208xA introduce a third level of cache. Does that level support locking?

0 件の賞賛
返信

2,756件の閲覧回数
Pavel
NXP Employee
NXP Employee

The LS208xA supports L3 cache locking.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信