CW4NET_v2020.06 Linux package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW4NET_v2020.06 Linux package

2,846 Views
madhu-krishnamurthy
Contributor I

Hi

I am having a problem with CW4NET_v2020.06 (linux  version) - the code warrior tap application for installing QSPI image on the LS2088a. When I open the tool,  the device list is empty as seen in the screen shot  - where it should have listed  LS2088a among other devices.  It was working  before but this happened after I moved the installation directory and I cannot get it to work now. Do you know how to  fix it ?

I want do a fresh install but I do not have the installation package. I can't find it on the nxp site. Can you please point me to it.

 

thanks

Madhu

 

Labels (1)
0 Kudos
Reply
1 Reply

2,842 Views
ufedor
NXP Employee
NXP Employee

Using the following CW4NET link:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

you need to search for:

CodeWarrior for ARMv8 v11.5.0 b200629 Linux Offline Installer
Last modified Jul 1, 2020
File Name CW_ARMv8_v2020.06_b200629GA_Linux_Offline.tar

and

CodeWarrior for ARMv8 v11.5.2 b210130 Linux Offline Update
Last modified Jan 29, 2021
File Name com.freescale.armv8.11.5.2.GA.Lin.updatesite.210130.zip

0 Kudos
Reply