CW SPD Read failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW SPD Read failure

1,587 次查看
akhilesh_nema
Contributor IV

I have a custom board based on LS1046A, with a DDR4 SODIMM and I am validating a new DDR4 module using the DDR validation tool. However, I can't read the SPD from the CW. The SPD_EEPROM_ADDRESS is 0x50, and SPD_BUS_NUM is 1. 

I have checked  C:\Freescale\CW4NET_v2020.06\Common\QCVS\Optimization\resources\QorIQ\ARMv8\templates\ddr\system_config_params_read_spd.json, The 0x50 is listed here but I cannot find a place to set the bus number.

 

 

 

        "in" : {
            "spd_eeprom_addrs" : "0x50 0x51 0x52 0x53 0x54 0x55 0x56 0x57",
            "i2c_mux_addrs" : "<<{I2C_MUX}>>",
            "i2c_mux_ch_default" : "0x8"
        },

 

 

 

"Read SPD" from DDR configuration tool does not work.  Probe connection is fine.

 

Screenshot 2025-02-21 060137.png

 

 

Screenshot 2025-02-21 054628.png

I have tried to manually setup the project by using a known working reg file (created for a different DDR CBD26D4S9S1KC-4 ) and then reading the SPD using FSL-DDR, and modified non matching settings, but that project has Validation failures, so I am trying to directly read the SPD from the CW.

 

 

FSL DDR>print dimm
SPD info:  Controller=0 DIMM=0
0      : 23 info_size_crc  bytes written into serial memory, CRC coverage
1      : 11 spd_rev        SPD Revision
2      : 0c mem_type       Key Byte / DRAM Device Type
3      : 03 module_type    Key Byte / Module Type
4      : 84 density_banks  SDRAM Density and Banks
5      : 19 addressing     SDRAM Addressing
6      : 00 package_type   Package type
7      : 08 opt_feature    Optional features
8      : 00 thermal_ref    Thermal and Refresh options
9      : 60 oth_opt_features Other SDRAM optional features
10     : 00 res_10         Reserved
11     : 03 module_vdd     Module Nominal Voltage, VDD
12     : 01 organization Module Organization
13     : 03 bus_width      Module Memory Bus Width
14     : 00 therm_sensor   Module Thermal Sensor
15     : 00 ext_type       Extended module type
16     : 00 res_16       Reserved
17     : 00 timebases    MTb and FTB
18     : 06 tck_min      tCKAVGmin
19     : 0d tck_max      TCKAVGmax
20     : f8 caslat_b1    CAS latencies, 1st byte
21     : 3f caslat_b2    CAS latencies, 2nd byte
22     : 00 caslat_b3    CAS latencies, 3rd byte
23     : 00 caslat_b4    CAS latencies, 4th byte
24     : 6e taa_min      Min CAS Latency Time
25     : 6e trcd_min     Min RAS# to CAS# Delay Time
26     : 6e trp_min      Min Row Precharge Delay Time
27     : 11 tras_trc_ext Upper Nibbles for tRAS and tRC
28     : 00 tras_min_lsb tRASmin, lsb
29     : 6e trc_min_lsb  tRCmin, lsb
30     : 20 trfc1_min_lsb  Min Refresh Recovery Delay Time, LSB
31     : 08 trfc1_min_msb  Min Refresh Recovery Delay Time, MSB
32     : 00 trfc2_min_lsb  Min Refresh Recovery Delay Time, LSB
33     : 05 trfc2_min_msb  Min Refresh Recovery Delay Time, MSB
34     : 70 trfc4_min_lsb Min Refresh Recovery Delay Time, LSB
35     : 03 trfc4_min_msb Min Refresh Recovery Delay Time, MSB
36     : 00 tfaw_msb      Upper Nibble for tFAW
37     : a8 tfaw_min      tFAW, lsb
38     : 18 trrds_min     tRRD_Smin, MTB
39     : 28 trrdl_min     tRRD_Lmin, MTB
40     : 28 tccdl_min     tCCS_Lmin, MTB
41 - 59: 00 78 00 14 3c 00 00 00 00 00 00 00 00 00 00 00 00 00 00
60 - 77: 0c 2b 2d 04 16 35 23 0d 00 00 2c 0b 03 24 35 0c 03 2d    mapping[] Connector to SDRAM bit map
117    : 00 fine_tccdl_min Fine offset for tCCD_Lmin
118    : 9c fine_trrdl_min Fine offset for tRRD_Lmin
119    : 00 fine_trrds_min Fine offset for tRRD_Smin
120    : 00 fine_trc_min   Fine offset for tRCmin
121    : 00 fine_trp_min   Fine offset for tRPmin
122    : 00 fine_trcd_min  Fine offset for tRCDmin
123    : 00 fine_taa_min   Fine offset for tAAmin
124    : e7 fine_tck_max   Fine offset for tCKAVGmax
125    : 00 fine_tck_min   Fine offset for tCKAVGmin
126-127: 64 20   SPD CRC
128    : 0f mod_height    (Unbuffered) Module Nominal Height
129    : 11 mod_thickness (Unbuffered) Module Maximum Thickness
130    : 00 ref_raw_card  (Unbuffered) Reference Raw Card Used
131    : 00 addr_mapping  (Unbuffered) Address mapping from Edge Connector to DRAM
254-255: 45 ad   Module CRC
320    : 07 Module MfgID Code LSB - JEP-106
321    : f7 Module MfgID Code MSB - JEP-106
322    : 00 Mfg Location
323-324: 24 39 Mfg Date
325-328: 09 23 00 02    Module Serial Number
329-348: 43 4d 42 36 2d 35 46 41 31 30 42 41 52 30 31 55 55 30 20 20    Mfg's Module Part Number
349    : 00 Module Revision code
350    : 80 DRAM MfgID Code LSB - JEP-106
351    : ce DRAM MfgID Code MSB - JEP-106
352    : 00 DRAM stepping
353-381: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    Mfg's Specific Data



DIMM parameters:  Controller=0 DIMM=0
DIMM organization parameters:
module part name = CMB6-5FA10BAR01UU0
rank_density = 4294967296 bytes (4096 megabytes)
capacity = 4294967296 bytes (4096 megabytes)
burst_lengths_bitmask = 0C
base_addresss = 0 (00000000 00000000)
n_ranks = 1
data_width = 64
primary_sdram_width = 64
ec_sdram_width = 0
package_3ds = 0
registered_dimm = 0
mirrored_dimm = 0
device_width = 8
n_row_addr = 15
n_col_addr = 10
edc_config = 0
bank_addr_bits = 0
bank_group_bits = 2
die_density = 0x00000004
tckmin_x_ps = 750
tckmin_x_minus_1_ps = 0
tckmin_x_minus_2_ps = 0
tckmax_ps = 1600
caslat_x = 2096128
caslat_x = 0x001FFC00
taa_ps = 13750
caslat_x_minus_1 = 0
caslat_x_minus_2 = 0
caslat_lowest_derated = 0
trcd_ps = 13750
trp_ps = 13750
tras_ps = 32000
tfaw_ps = 21000
trfc1_ps = 260000
trfc2_ps = 160000
trfc4_ps = 110000
trrds_ps = 3000
trrdl_ps = 4900
tccdl_ps = 5000
trfc_slr_ps = 0
trc_ps = 45750
refresh_rate_ps = 7800000
dq_mapping[0] = 0x0000000C
dq_mapping[1] = 0x0000002B
dq_mapping[2] = 0x0000002D
dq_mapping[3] = 0x00000004
dq_mapping[4] = 0x00000016
dq_mapping[5] = 0x00000035
dq_mapping[6] = 0x00000023
dq_mapping[7] = 0x0000000D
dq_mapping[8] = 0x00000000
dq_mapping[9] = 0x00000000
dq_mapping[10] = 0x0000002C
dq_mapping[11] = 0x0000000B
dq_mapping[12] = 0x00000003
dq_mapping[13] = 0x00000024
dq_mapping[14] = 0x00000035
dq_mapping[15] = 0x0000000C
dq_mapping[16] = 0x00000003
dq_mapping[17] = 0x0000002D
dq_mapping_ors = 1



"lowest common" DIMM parameters:  Controller=0
tckmin_x_ps = 750 (1333 MHz)
tckmax_ps = 1600 (625 MHz)
all_dimms_burst_lengths_bitmask = 0C
taamin_ps = 13750
trcd_ps = 13750
trp_ps = 13750
tras_ps = 32000
trfc1_ps = 260000
trfc2_ps = 160000
trfc4_ps = 110000
trrds_ps = 3000
trrdl_ps = 4900
tccdl_ps = 5000
trfc_slr_ps = 0
twr_ps = 15000
trc_ps = 45750
refresh_rate_ps = 7800000
extended_op_srt = 0
lowest_common_spd_caslat = 11
highest_common_derated_caslat = 0
additive_latency = 0
ndimms_present = 1
all_dimms_registered = 0
all_dimms_unbuffered = 1
all_dimms_ecc_capable = 0
total_mem = 4294967296 (4096 megabytes)
base_address = 0 (0 megabytes)


User Config Options: Controller=0
cs0_odt_rd_cfg = 0
cs0_odt_wr_cfg = 4
cs1_odt_rd_cfg = 0
cs1_odt_wr_cfg = 0
cs2_odt_rd_cfg = 0
cs2_odt_wr_cfg = 0
cs3_odt_rd_cfg = 0
cs3_odt_wr_cfg = 0
cs0_odt_rtt_norm = 3
cs0_odt_rtt_wr = 0
cs1_odt_rtt_norm = 0
cs1_odt_rtt_wr = 0
cs2_odt_rtt_norm = 0
cs2_odt_rtt_wr = 0
cs3_odt_rtt_norm = 0
cs3_odt_rtt_wr = 0
memctl_interleaving = 0
memctl_interleaving_mode = 0
ba_intlv_ctl = 0x00000000
ecc_mode = 1
ecc_init_using_memctl = 1
dqs_config = 0
self_refresh_in_sleep = 1
dynamic_power = 0
data_bus_width = 0
burst_length = 6
cas_latency_override = 0
cas_latency_override_value = 3
use_derated_caslat = 0
additive_latency_override = 0
additive_latency_override_value = 3
clk_adjust = 8
cpo_override = 0
write_data_delay = 0
half_strength_driver_enable = 0
twot_en = 0
threet_en = 0
registered_dimm_en = 0
mirrored_dimm = 0
ap_en = 0
x4_en = 0
package_3ds = 0
bstopre = 0
wrlvl_override = 1
wrlvl_sample = 15
wrlvl_start = 17
cswl_override = 0x00000000
rcw_override = 0
rcw_1 = 0x00000000
rcw_2 = 0x00000000
rcw_3 = 0x00000000
ddr_cdr1 = 0x80040000
ddr_cdr2 = 0x000000C1
tfaw_window_four_activates_ps = 21000
trwt_override = 0
trwt = 0
rtt_override = 0
rtt_override_value = 0
rtt_wr_override_value = 0


Address Assignment: Controller=0 DIMM=0
Don't have this functionality yet


Computed Register Values: Controller=0
cs0_bnds = 0x000000FF
cs0_config = 0x80040322
cs0_config_2 = 0x00000000
cs1_bnds = 0x00000000
cs1_config = 0x00000000
cs1_config_2 = 0x00000000
cs2_bnds = 0x00000000
cs2_config = 0x00000000
cs2_config_2 = 0x00000000
cs3_bnds = 0x00000000
cs3_config = 0x00000000
cs3_config_2 = 0x00000000
timing_cfg_3 = 0x010C1000
timing_cfg_0 = 0x91550018
timing_cfg_1 = 0xBAB48E44
timing_cfg_2 = 0x00490111
ddr_sdram_cfg = 0xC5000000
ddr_sdram_cfg_2 = 0x00401150
ddr_sdram_cfg_3 = 0x00000000
ddr_sdram_mode = 0x03010211
ddr_sdram_mode_2 = 0x00000000
ddr_sdram_mode_3 = 0x00010211
ddr_sdram_mode_4 = 0x00000000
ddr_sdram_mode_5 = 0x00010211
ddr_sdram_mode_6 = 0x00000000
ddr_sdram_mode_7 = 0x00010211
ddr_sdram_mode_8 = 0x00000000
ddr_sdram_mode_9 = 0x00000500
ddr_sdram_mode_10 = 0x00400000
ddr_sdram_mode_11 = 0x00000400
ddr_sdram_mode_12 = 0x00400000
ddr_sdram_mode_13 = 0x00000400
ddr_sdram_mode_14 = 0x00400000
ddr_sdram_mode_15 = 0x00000400
ddr_sdram_mode_16 = 0x00400000
ddr_sdram_interval = 0x18600000
ddr_data_init = 0xDEADBEEF
ddr_sdram_clk_cntl = 0x02000000
ddr_init_addr = 0x00000000
ddr_init_ext_addr = 0x00000000
timing_cfg_4 = 0x00220002
timing_cfg_5 = 0x03401400
timing_cfg_6 = 0x00000000
timing_cfg_7 = 0x13300000
timing_cfg_8 = 0x01224800
timing_cfg_9 = 0x00000000
ddr_zq_cntl = 0x8A090705
ddr_wrlvl_cntl = 0x8675F611
ddr_wrlvl_cntl_2 = 0x06000000
ddr_wrlvl_cntl_3 = 0x00000000
ddr_sr_cntr = 0x00000000
ddr_sdram_rcw_1 = 0x00000000
ddr_sdram_rcw_2 = 0x00000000
ddr_sdram_rcw_3 = 0x00000000
ddr_cdr1 = 0x80040000
ddr_cdr2 = 0x000000C1
dq_map_0 = 0x32BB4458
dq_map_1 = 0xD6336C2C
dq_map_2 = 0x0E4D4C0C
dq_map_3 = 0xB4000001
err_disable = 0x00000000
err_int_en = 0x00000000
ddr_eor = 0x00000000
debug_01 = 0x00000000
debug_02 = 0x00000000
debug_03 = 0x00000000
debug_04 = 0x00000000
debug_05 = 0x00000000
debug_06 = 0x00000000
debug_07 = 0x00000000
debug_08 = 0x00000000
debug_09 = 0x00000000
debug_10 = 0x00000000
debug_11 = 0x00000000
debug_12 = 0x00000000
debug_13 = 0x00000000
debug_14 = 0x00000000
debug_15 = 0x00000000
debug_16 = 0x00000000
debug_17 = 0x00000000
debug_18 = 0x00000000
debug_19 = 0x00000000
debug_20 = 0x00000000
debug_21 = 0x00000000
debug_22 = 0x00000000
debug_23 = 0x00000000
debug_24 = 0x00000000
debug_25 = 0x00000000
debug_26 = 0x00000000
debug_27 = 0x00000000
debug_28 = 0x00000000
debug_29 = 0x00700061
debug_30 = 0x00000000
debug_31 = 0x00000000
debug_32 = 0x00000000
debug_33 = 0x00000000
debug_34 = 0x00000000
debug_35 = 0x00000000
debug_36 = 0x00000000
debug_37 = 0x00000000
debug_38 = 0x00000000
debug_39 = 0x00000000
debug_40 = 0x00000000
debug_41 = 0x00000000
debug_42 = 0x00000000
debug_43 = 0x00000000
debug_44 = 0x00000000
debug_45 = 0x00000000
debug_46 = 0x00000000
debug_47 = 0x00000000
debug_48 = 0x00000000
debug_49 = 0x00000000
debug_50 = 0x00000000
debug_51 = 0x00000000
debug_52 = 0x00000000
debug_53 = 0x00000000
debug_54 = 0x00000000
debug_55 = 0x00000000
debug_56 = 0x00000000
debug_57 = 0x00000000
debug_58 = 0x00000000
debug_59 = 0x00000000
debug_60 = 0x00000000
debug_61 = 0x00000000
debug_62 = 0x00000000
debug_63 = 0x00000000
debug_64 = 0x00000000


FSL DDR>

 

 

 

 

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,550 次查看
yipingwang
NXP TechSupport
NXP TechSupport

For reading from SPD, would you please click "X" and send the whole error log to me?

0 项奖励
回复