CMSIS-DAP vs JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS-DAP vs JTAG

1,609件の閲覧回数
TrinathK
Contributor III

Hi,

We are designing PCB board for our application that uses ls1043a processor. For programming and debugging purpose, we want to go with JTAG interface instead of CMSIS-DAP interface due to the board space constraint.

Let me know if it is OK to use JTAG instead of CMSIS-DAP.

If "No" is the answer, please tell me the proper reason for it and also let me know what are all the additional features available in CMSIS-DAP.

Thanks in advance.

0 件の賞賛
返信
1 返信

1,603件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Let me know if it is OK to use JTAG instead of CMSIS-DAP.

CMSIS-DAP is an optional module - i.e. JTAG can be used for the board bring-up solely.